SDI-12 connector to the ProSample
Item 630125 can be installed at the end of an SDI-12 cable such as the EXO flying lead cable (item # 599008 ). This allows for connection of an SDI-12 cable to a ProSample P-12 or ProSample PM-12.Please note there is no cable included with this item. This connector is the same ProSample connector pre-installed on the 630146 and 630145 ProSample SDI-12 cables.Please see the ProSample Ordering Guide if ordering a complete system, or contact us if you have any questions.