It looks like you are coming from United States, but the current site you have selected to visit is Europe. Do you want to change site?

Yes, please! No, keep me on the current site

Enable high contrast mode
See All Defender® Regenerative Media Filter

Defender® Regenerative Media Filter

  • is the minimum order quantity for this product. Please check quantity and add to cart again.

Request a Proposal

*  Required Field

Award winning Defender® regenerative media filtration (RMF) systems are capable of filtering particulate down to 1 micron and require no backwash.

Looking to make the jump from sand filtration to RMF technology? Experience up to;

  • 90% Water Savings
  • 50% Energy Savings
  • 30% Chemical Savings
  • 75% Space Savings
  • 95% Less Particulate

The Defender® regenerative media filter provides exceptional water filtration capabilities, along with significant water and energy savings when compared to sand filtration. It has rapidly replaced sand filters as the premier choice for water filtration in various recreational water applications.

Regenerative media filters provide substantial savings in the everyday operational costs of an aquatics facility. To highlight potential savings, Neptune Benson can evaluate your current facility (or upcoming project) and demonstrate a cost saving analysis report, outlining the savings in water, energy, chemical consumption and required footprint when compared to a conventional sand filter.

Due to its innovative "bumping" process the Defender® RMF systems significantly eliminate the amount of backwash water going to the drain. Instead of backwashing, the Defender filter is programmed to automatically “bump” to regenerate the fine-grade perlite media for a fresh start. After approximately 4 weeks of "bumping" the perlite may be saturated with dirt particles and require a quick media replacement.

The Defender RMF technology represents what it truly means to be a compact filter. The small footprint requirement results in as little as one-fourth to one-sixth of the space required by an equivalently sized sand system, saving on installation costs, rigging time and more. With a much lower operating weight, the Defender filter reduces the extent to which the floor slab must be engineered. When building costs are at an estimated $75 to $150 per square foot, selecting a Defender filter could generate construction savings in the tens of thousands of dollars. In older facilities where expanding the footprint is not an option, this technology will enable you to achieve your goals while utilizing your current footprint.

The Defender® filter reduces head loss when compared to traditional sand filters, ultimately saving motor horsepower operational costs. Starting differential pressures for a high-rate sand filter, depending on the media, could range from 4 to 6 psi (27.6 kpa to 41.4 kpa). In contrast, the starting differential of the Defender filter is approximately 1 psi (6.9 kpa).

Converting this to head represents savings of nearly 12 feet (3.65m) total dynamic head, or TDH, which directly translates to horsepower and energy savings. For example utilizing a 25hp motor instead of a 30hp unit would result in electricity savings of $3,000 per year.

The Defender filter removes particles down to 1 micron in size. With the growing concerns of recreational waterborne illnesses (RWI) such as cryptosporidiosis, the smaller the particle removal the better the water quality and safety of your bathers. The Defender filter is especially effective on pools with heavy bather loads because of the increased filter area and dirt holding capacity.

With its fine filtration capabilities the Defender filter will also delay the increase in turbidity. The high-performance filtration capabilities, along with the reduction of make-up water due to minimizing backwash cycles, reduces the chemical requirements and the associated turbidity buildup.

Findings from a recent study by the University of North Carolina on cryptosporidium and particle removal from swimming pool water indicate:

  • Precoat Filtration with both DE and perlite outperformed cartridge and sand filtration by a wide margin.
  • Single pass testing resulted in crypto removal of 99.9% using perlite media.
  • When testing 1-micron microsphere removal, perlite performed at 56.5% versus 20.2% for sand.

The dramatic reduction of backwash waste directly translates to savings in make-up water along with the chemicals and fuel for re-heating. Consider the cost of chemically treating 1.4 million gallons and the BTU’s required to heat this volume from 50 degrees (10 °C) to 80 degrees Fahrenheit (27 °C).

It is also important to note that the improved water quality generated by the Defender® filter's ability to remove finer particles will also save on general chemical consumption.

Estimated annual savings ranges from $42,000 to $52,000 depending on local fuel costs for oil, gas or electricity. This is based on the backwash water consumption of a typical waterpark attraction with a 2000 GPM (454m3 /hr) recirculation rate.

Related Products