It looks like you are coming from United States, but the current site you have selected to visit is China. Do you want to change sites?

Yes, please. No. Keep me on the current site.

optimyze Configuration

No configurations are needed for optimyze. The user must enter the following data while adding the device in the Secure Connect application.

Parameter Description
Device type optimyze
Name A name for the device
Serial number The serial number that is located below the QR code on the device, and in the optimyze mobile application