It looks like you are coming from United States, but the current site you have selected to visit is China. Do you want to change sites?

Yes, please. No. Keep me on the current site.

Hydrovar X configuration for Xylem Vue Secure Connect

On the Hydrovar X device, the up and down key must be pressed to change the submenus.

  1. Go to the communication settings at M08.
  2. Set the following parameters.
ID Parameter Setting
P08.0.02 Com 2 Function 1-Modbus
P08.1.01 Address 1-127
P08.1.02 Baudrate 115200 bps
P08.1.08 RTU Format 8, N,1
Format = 8 bits
Parity = None
Stop bits = 1