It looks like you are coming from United States, but the current site you have selected to visit is China. Do you want to change sites?

Yes, please. No. Keep me on the current site.

Configure MultiSmart

Use the MultiSmart HMI to configure the MultiSmart device. Contact Xylem support to get the applicable data points.

CCD gateway connection:

  1. Go to Settings > Communication > Protocol Settings > Modbus Slave.
  2. Set the communication parameters.

    Parameter Setting
    Modbus address 1
    Baud 9600
    Stop bits 1
    Data bits  8
    Parity None


    Cloud gateway connection:

    MultiSmart must be onboarded before installation to Secure connect. Contact Xylem support if the MutliSmart is not onboarded.
    Multi-smart device can share IP address. Assign each device a unique outstation address or TCP port.