Changing Nutrient Monitoring Forever
EXO NitraLED is the world’s most accessible UV Nitrate sensor, built with state-of-the-art LED technology, for long-term nutrient monitoring.
ProSample for COVID RNA Detection
With 12 programmable settings, users can configure the instrument to collect wastewater samples, which provides the most accurate representation of the residents in the building and the potential presence of COVID-19.
Vertical Profiling Systems (VPS)
5 Deployment Configurations - Ocean, Pontoon, Fixed, Mini and Aerial provide a reliable, fully-automated data collection platform for the early warning of intrusion events for business and environmental critical decision making
ProSolo Optical Dissolved Oxygen Meter
The ProSolo incorporates smart sensor technology that enables sensors to be automatically recognized by the handheld. Additionally, DIGITAL sensors store calibration data, so probe assemblies can be swapped between handhelds without the need for re-calibration.
Featured Products
- ProDigital System ProDSS Multiparameter Water Quality Meter The ProDSS multiparameter water quality meter measures a variety of parameters and is the most...
- EXO Platform EXO NitraLED UV Nitrate Sensor Utilizing state-of-the-art UV LED technology, EXO NitraLEDâ„¢ is an optical nitrate sensor designed...
- Multiparameter Sondes EXO2 Multiparameter Sonde
- ProDIGITAL System ProSolo Digital Water Quality Meter Digital water quality meter designed to interface with digital smart sensors for dissolved oxygen,...
- 2900M Online Monitor & Control System The YSI 2900M Online Monitoring and Control System featuring the YSI Sitini Online Sampler is a key...
- i3XO EcoMapper AUV The next generation of autonomous water quality vehicles. The i3XO generates high-resolution maps...