It looks like you are coming from United States, but the current site you have selected to visit is Japan. Do you want to change sites?

Yes, please. No. Keep me on the current site.

Using the pump in different water sources

Your LORENTZ solar water pump is flexible and can pump from almost any water source. If you are using it in a source where the pump might not be upright all the time (such as a river or pond), please be aware that in this case the dry run protection should not be attached to the pump. For more information on how to use a dry run protection in this circumstance, please read this article:

Function and use of dry run protection

Examples for possible water sources are:

Wells

Ponds

Rivers