-
Xylem as turnkey contractor for the new pumping stations in Bromstensstaden
Urban development in Bromstensstaden required new, reliable wastewater pumping stations to meet increased demands on the water and wastewater system. -
Xylem as turnkey contractor for a new pumping station solution in Kristvallabrunn
Xylem delivered a turnkey pumping solution in Kristvallabrunn, including a new pumping station and booster station for reliable, energy-efficient wastewater transfer. -
Satellite manufacturer achieves zero liquid discharge with Xylem
A Texas-based satellite manufacturer solved the challenge of no sewer access by deploying a zero liquid discharge water recycling system. The solution enables 95%+ water reuse, recovers 66M gallons annually, and avoids $30M+ in disposal costs, while digital monitoring ensures reliable, uninterrupted satellite production and strong sustainability performance. -
ApaVital S.A.: Reduction of daily water losses by over 800 m³
ApaVital deploys Xylem Vue to reduce daily water losses by over 800 cubic meters, achieving compliance with EU regulations. -
Driving precision and sustainability in agri-tech
Learn how Sentec developed calibration free agricultural flow meters in record time boosting accuracy reducing waste improving yields and supporting sustainable farming -
Predicting failure: smart fault detection for underground cable networks
Sentec partnered with a leading solutions provider to develop a scalable monitoring system that predicts and accurately locates faults in underground cable networks, enabling faster and more cost-effective maintenance. -
Advancing carbon capture: sensor technology to monitor safely and at scale
Discover how Sentec partnered with a leading CCS operator to identify sensor technologies and integration pathways for safe, scalable CO₂ monitoring, enabling safer long‑term storage, reduced operational complexity, and regulatory‑ready deployment strategies. -
Stadtwerke Trier: AI-aided energy optimization for daily energy balancing
Xylem Vue helped Stadtwerke Trier optimize renewable energy use in its drinking water network, achieving 90% self-consumption. -
Critical pipe repair: Smith-Blair adapters help Canadian sawmill
See how custom Smith-Blair 935/936 adapters repaired deteriorated concrete pipe at a Canadian sawmill without service interruption. Read the full case study. -
Out-of-Round pipe emergency repair
How Smith-Blair custom-engineered 624 MJ tapping sleeves solved a 5/8" out-of-round pipe challenge on aging ductile iron infrastructure in Florida. -
Emergency sewer system repair
40-year-old carbon steel pipe with catastrophic failure repaired in hazardous wet well conditions. Smith-Blair 675 restored system integrity with zero downtime. -
Pump Station in Krokom – Unique PE Construction
Xylem delivered a turnkey solution for one of Sweden’s first pump stations featuring a fully integrated PE construction in Krokom. -
Eau d’Azur: France’s first smart water network cuts losses and strengthens drought resilience
The Metropolis of Nice is implementing a hypervision platform, based on Xylem Vue technology, to increase efficiency, sustainability, and resilience by providing a real-time view of the network. -
Thames Water and Xylem set new standard for pump upgrades at scale
A Xylem and Thames Water partnership represents a shift in how water companies can manage inherited infrastructure. -
Scottish Water cuts energy by 60% with Flygt Concertor intelligent pump system
Scottish Water partnered with Xylem to upgrade hundreds of pumping stations with innovative, energy-efficient technology, as part of its commitment to reaching net-zero emissions. -
Herford utility: cutting CSOs by around 15% using an advanced prevention system
Inconsistent behavior and utilization of control structures was observed for past rainfall events. The municipality decided that an optimized network control system should be implemented to better utilize existing retention volumes, coordinate them effectively and reduce water pollution.
-
Alberta Utility Averts Potential Catastrophic Holiday Failure with Proactive Pipeline Management Approach
To ensure safe and reliable water service for its customers, EPCOR partnered with Pure Technologies, a Xylem brand to complete a high-resolution condition assessment. The team inspected a 9.4-kilometer (5.8-mi) section of the critical Northside Pipeline for leaks and pipe wall deterioration.
-
Xylem bypass system helps facilitate pump station upgrades
Allegheny County Sanitary Authority (ALCOSAN) is a municipal authority that provides wastewater treatment services to 83 communities, including the city of Pittsburgh, reaching a total population of 1.2 million people. -
Welsh Water scales up Xylem’s Flygt Concertor for smarter wastewater management
Dŵr Cymru Welsh Water is scaling up its deployment of Flygt Concertor intelligent pumping systems to improve wastewater network resilience, reduce energy consumption, and support its environmental goals. -
State of the art water treatment technology for a forging works in Saxony, Germany
Various cooling towers are operated in the water treatment plant at the forge. Disinfection is carried out using expensive biocides, which are also environmentally problematic for rivers when discharged directly. The company was therefore looking for new, efficient and cost-effective disinfection technology to solve these issues. -
Nanobubbles enable Meister Cheese to increase cheese & biogas production
Meister Cheese improved wastewater treatment and biogas production using Moleaer's nanobubble technology, saving $10M in CAPAX improvements and doubling cheese output. -
Foul odors eliminated using nanobubble technology at a poultry processor
Miller Poultry cut foul lagoon odors and improved water quality using Moleaer's nanobubble technology, solving odor issues and boosting treatment efficiency. -
Maximizing biogas production through effective mixing technology and active seal protection
Learn more about maximizing biogas production through effective mixing technology and active seal protection. Read our case study with our customer Nesemeier now →
-
Sustainability success for Dairygold: mixers deliver biogas system results that matter
Flygt mixers deliver sustainable success for Dairygold at the heart of the world's largest ADI-BVF® fermenter. Read the case study →