-
Xylem Watermark teams with Water Well Trust to install new water well for Texas family
The cost of caring for a daughter with cerebral palsy created a challenge for the Salazars to finance and build a well on their modest income. For more than two decades, the family has made do with sharing water from the well located on the neighboring property owned by Nancy’s parents.
-
EWE WASSER GmbH: application of a real-time assistance system to reduce aeration energy usage and minimize operational expenses
Xylem Vue has helped to reduce Cuxhaven’s WWTP aeration energy requirements by over 26% and meet its effluent quality requirements.
-
Tuas Power Singapore identifies and eliminates harmful transients to improve system reliability and prolong the effective life of infrastructure assets
The power utility supplies high grade water for their own internal processes as well other industrial customers. Tuas Power was experiencing leaks within their distribution network, which were unexpected because these pipelines were less than five years old, made of steel, and laid above ground.
-
Nordic City Takes Proactive Approach to Reduce NRW While Gaining Valuable Condition Assessment Data on Critical Water Mains, Avoiding Costly Failures
As part of a pre-emptive program to address non-revenue water loss and understand the condition of their pipes, Gothenburg wanted to conduct a condition assessment and leak detection survey on a series of large diameter transmission mains. The three pipelines were built in the 1960s and made of cement and steel, ranging in size from 1000 mm to 1200 mm.
-
Utility reduces CSO volume by 80%, saving $400 million in CapEx spending using “smart sewer” technology
Predictive monitoring and automated control optimized combined sewer operations, reducing overflow volumes and deferring major capital infrastructure investment.
-
Flower Mound, Texas Prioritizes Repairs, Prevents Failures, and Reduces Risk with Engineering Assessment
The assessment was urgent, as Flower Mound planned to widen a major road next to the main and wanted reliable information on the condition of that particular pipeline before the road was built. Any necessary repairs or replacement needed to be completed prior to construction to avoid significant disruption and additional expense.
-
-
Wholesale Water Supplier Takes Proactive Approach to Managing High-Value Metallic Transmission Mains
-
Grand Rapids, Michigan saves 800K through large valve assessment
Over the last few years, the operation and maintenance of the large valves had declined due to focus being placed on other critical priorities. Without a consistent exercise routine for critical valves, the utility found that many of these valves were inoperable and, as a result, began to seek funding for valve replacements.
-
Grand Rapids, Michigan saves one billion dollars as real-time decision support system solves infiltration and inflow problem
After nearly 25 years, Grand Rapids finished retrofitting its combined sewer overflow system to a separate sanitary and stormwater system, completing its long-term control plan (LTCP) in 2015. But now, the City needed to get a better understanding of the infiltration and inflow into these newly separated sanitary sewers to ensure compliance with a mandate from the Michigan Department of Environmental Quality (DEQ).
-
-
-
A custom bulk dewatering system for 100% compliance
A North American power utility needed to dewater wet fly ash ponds at sites without permanent power. Xylem engineers created a modular system that combined different products into a single streamlined solution.
-
Remote monitoring & controls for unmanned reliability
Xylem was tasked with designing a seep collection system to collect water from a low volume seep through the wall of a decommissioned fly ash pond. The sump was located in an active river floodplain that flooded with as little as 1-2 inches of rain, so the customer needed an automatic shutdown when the river covered the sump.
-
-
-
Clayton County, Georgia reduces apparent water loss & identifies one million in recoverable revenue
Clayton County Water Authority (CCWA) is a good example of a utility that doesn’t let a confined geographical footprint stop it from thinking outside the box. As one of Georgia’s smallest counties in terms of land size area (only 143 square miles), its location near the top of a regional watershed means it has little area to gather precipitation into streams and rivers.
-
-
UV treatment system fills the bill for water reuse
Although St. Francis, Minnesota, located in Anoka and Isanti counties, has a population of only 7,218, it has big ideas when it comes to the future of its wastewater treatment system. Those big ideas came to fruition starting in 2015 when the city began building a new treatment facility at its existing wastewater treatment plant, which was built in the 1970s. Although upgraded in 2000, the upgrade did not address existing and future regulations regarding ammonia and phosphorus.
-
-
-
-
-