It looks like you are coming from United States, but the current site you have selected to visit is Kosovo. Do you want to change site?

Yes, please! No, keep me on the current site

Aquavar IPC Enclosure

One of the advantages of the new Aquavar Intelligent Pump Controller (IPC) is the flexibility to use the drive in many different applications. Whether it is a borehole application requiring outdoor enclosure or surface mount pump and motor requiring a drive to withstand corrosive environment, the IPC has the right solution. Each drive enclosure is constructed to provide a different degree of protection to personnel against access to hazardous parts. The following table is meant to serve as a quick reference tool to easily compare and contrast different types of enclosures as well as to provide some general applications to help specify selection.