It looks like you are coming from United States, but the current site you have selected to visit is Kosovo. Do you want to change site?

Yes, please! No, keep me on the current site

Flygt Channel Impeller Pumps

C-3000

CHANNEL IMPELLER PUMPS

  • Non-clog impellers
  • Single and multi-vane designs
  • Traditional large throughlet designs
  • High clean water efficiencies
  • ​Cast iron and optional impeller materials

Need help?

Contact an Expert

Contact an Expert

Whether you would like additional information or are interested in getting a quote, we're here to help.

All fields required.

*  Required Field
Pump Models Technology Case Studies & White Papers
Pump Models
There are no results that match your search
Technology

FLYGT CHANNEL IMPELLER PUMPS

Flygt Channel impeller C-pumps are built to handle capacities of up to 3,000 l/s (48000 gpm) with motors up to 775 kW (1050 hp). The base versions of these pumps are made in durable cast iron and are intended for demanding applications such as municipal sewage and industrial effluent. Explosion-proof versions are available. The classic C-pumps with shrouded single and multivane impellers have proven themselves over the years. The smaller C-pumps are equipped with the Flygt Nevaclog® impeller, which has large free passage solids-passing properties. The larger pumps have multi-vane impellers for maximum hydraulic efficiency and clog resistance.

Case Studies & White Papers

Circular stormwater pump station

FRANCE

Challenge One of the largest airports serving France required a stormwater treatment plant to handle the inflow from a large gravity sewer collecting water from the runways. Solution The pump station...

Read More

Pump station with cleaning function

SWEDEN

Challenge Eighteen Flygt pump stations transport wastewater at a popular recreational and amusement area in central Stockholm. One of the pump stations handles restaurant wastewater containing fats,...

Read More

Expansion of a desalination plant

AUSTRALIA

Challenge One of Australia’s largest cities was running short of fresh water and needed a major expansion of its desalination facility. One hurdle was to transfer the seawater to the plant. A new...

Read More

Sewage and stormwater pump stations

UK

Storm water pump station design Challenge The revival of one of Britain’s largest commercially unexploited land areas called for multi-phase construction of two large pump stations. One pump station...

Read More

Large capacity circular wet well

USA

Challenge Very deep, large capacity and limited footprint: these are common demands by customers for their pump stations designs. Recently, two such pump stations were needed in the US. Solution The...

Read More

Circular wastewater lift station

USA

Challenge A 54,000-acre service area in a major city in Texas required assistance to handle a projected 50% increase in population and subsequent increase in wastewater processing demands. Solution...

Read More