It looks like you are coming from United States, but the current site you have selected to visit is United Kingdom. Do you want to change sites?

Yes, please. No. Keep me on the current site.

Flowmeters to look out for in 2018: The Xylem Flygt EMF801 MagFlux Flowmeter and MagFlux Quad

5 June 2018

Xylem, a leading global specialist in water technologies, has launched two new flowmeters: the MagFlux Quad and the WRAS and MCERTS approved Flygt EMF801 MagFlux Flowmeter. Providing an accurate solution for flow measurement in pipes, the systems seamlessly integrate with Flygt’s range of pumps and control devices, as Andrew Welsh, ICA general manager, explains.

For any industrial process that handles liquid or gas, measuring flow is a necessity. It ensures that the right fluid is in the right place, at the right time and it keeps employees and vital equipment safe.

The Flygt EMF801 MagFlux and MagFlux Quad Flowmeters represent a good choice for anyone who values accuracy, usability, flexibility and low maintenance when measuring flow.

The Flygt EMF801 MagFlux Flowmeter and the MagFlux Quad offer an accuracy of 0.25 per cent, even when measuring slow flow velocity as low as 0.2m/sec, through to highs of 10m/sec. The in-built data logger is capable of recording 20,000 entries, giving both an accurate and a consistent reading when measuring flow where space is a premium. Minimum pipe diameter for accurate flow on MagFlux EMF801 3 x Diameter inlet and 2 x Diameter outlet and on the MagFlux Quad only 1 x Diameter inlet and 1 x Diameter outlet.

Designed with flexibility in mind, the Flygt EMF801 MagFlux Flowmeter and the MagFlux Quad come in a full range of sizes, from DN20 (3/4”) to DN1200 (48”). To further meet the needs of a variety of applications, both Flygt flowmeters are also available with compact or remote mount design. This means that the intuitive, 5-line menu display can be fitted up to 1000 metres away from the sensor, if space restrictions are a challenge. For processes that involve a high level of flow, the display can withstand submersion in a depth of up to 10 metres (30 feet).

For busy process engineers, ease of installation is key, for an accurate measurement. Thanks to the unique MagFlux calibration code, the Flygt Flowmeters are quick and easy to commission, getting the system up and running easily and efficiently. Once operating, the Flygt Flowmeters are also capable of detecting when the pipe is empty and will alert operators to prevent breakdown and avert false flow calculations. Maintenance time is further cut by the system’s automatic electrode cleaning, which is active as standard.

Flow measurement isn’t glamorous, but it’s something that needs to be done. Investing in Xylem Flygt Flowmeters makes this job as easy, and as automatic, as possible.