It looks like you are coming from United States, but the current site you have selected to visit is Uganda. Do you want to change site?

Yes, please! No, keep me on the current site

Residential

Improving the quality of everyday living

Areas where private homes dominate, as opposed to industrial and commercial areas, are defined as residential areas. They can be anything from mobile homes to single- or multi-family housing developments. Independent of which type of residential area it is, the wastewater needs to be taken, collected and transported in some way. Depending on if it is urban or rural areas, vacation homes or permanent residencies and other factors different solutions are possible. They range from individual private treatment plants to different types of collection systems transporting the wastewater to a larger treatment plant.

Independent of the system, the residents depend on reliable products and a sound pump system design, making sure the wastewater is removed in a safe way, without effecting the living conditions or the environment.at minimal cost to the homeowner.

Drainage
Residential Drainage
Wastewater
Residential Wastewater
Hot Water Systems
Residential Hot Water Systems
Water Pressure
Residential Water Pressure
HVAC
Residential HVAC