It looks like you are coming from United States, but the current site you have selected to visit is Tajikistan. Do you want to change site?

Yes, please! No, keep me on the current site

Enable high contrast mode

Reducing the amount of water pumped / Adjusting motor speed

If the water flow is too high for your application, there is an easy way to limit the flow with the S-Connect app.

To lower the water flow you simply reduce the motor speed.

To do this, follow these steps:

  • open the S-Connect app and select "Settings"
  • turn on "Speed Limit"
  • now use the slider to adjust the speed according to your needs.

Further reading

Downloading the S-Connect app