It looks like you are coming from United States, but the current site you have selected to visit is Tajikistan. Do you want to change site?

Yes, please! No, keep me on the current site

Case Studies

Case Studies

  • Reliability and resilience: the key words for Mosswood

    Northumbrian Water provides water supply and sewerage services to a population of 2.7m in the north east and 1.8m in the south east of England, delivering 1,100 MLD of drinking water. Potable water treatment works vary from small groundwater sources to large surface water treatment facilities. Their Mosswood Water Treatment Works in County Durham treats 135 MLD of water by clarification, filtration and chlorination.
  • Stillorgan Reservoir disinfection upgrade

    Whilst residual chlorination is relied upon to provide protection of drinking water in distribution systems, it is increasingly being supplemented by ultraviolet (UV) irradiation as a primary disinfectant for drinking water treatment. As a chemical-free process it avoids many of the issues associated with hazardous oxidising disinfectants and does not generate disinfection by-products. It is also effective against microbiological pollutants such as protozoa, that are resistant to chlorine.
  • Updating London’s drinking water network

    A UK water supply company serves a population of approximately 675,000 consisting of homes and businesses in Surrey, Sussex and Kent and is a key part of London’s drinking water network. The largest works in Kent, which takes raw water from a reservoir that is recharged in winter by abstraction from the River Eden. The original works capacity was 35Ml/d and it is currently undergoing a phased uprate.
  • UV disinfection ensures compliance and improves water quality

    Irish Water was created by the Irish Government in 2013 and supplies drinking water to the whole of the Republic of Ireland. The company is investing over €65 million as part of their National Disinfection Programme involving the upgrade and standardisation of disinfection systems currently installed in over 800 sites including water treatment plants, pumping stations and reservoirs.
  • Water plants merged into a united plant with two pumping plants

    Wassergewinnung Essen (WGE) was founded in 2002 as a co-operative group between Essen Public Services and GELSENWASSER. At the Ruhr in Essen, the company is focused on procurement, extraction, treatment and supply of drinking water and then delivering to its partners.
  • Water works modernizes and upgrades treatment facility

    The German Echthausen Water Works is one of eight water works of Wasserwerke Westfalen GmbH, located in Dortmund, Germany. It was built in 1942. Wasserwerke Westfalen is a subsidiary company of both Dortmunder Energie- und Wasserversorgung GmbH and Gelsenwasser AG, and is the largest producer of drinking water in the German state of North Rhine-Westphalia.
  • UV solution mitigates microbiological corrosion for CEMEX

    Xylem was approached by CEMEX UK to supply a containerized ATG™ UV wastewater treatment plant to disinfect 125 m3/hr of effluent wastewater which would protect against the microbial induced corrosion of their pipe work and equipment.
  • UV disinfection eliminates chloramine issue at UK aquatic facility

    The Gloucester Institute of Technology operates an on-campus swimming and leisure facility and required a solution to its poor water quality due to high levels of chloramines, which are the cause of sore red eyes, itchy skin, overpowering chemical smells and is linked to cases of asthma in young children. Eliminating chloramines and maintaining water quality is a challenge for any leisure facility operator.
  • Ozone disinfection & sanitization upgrade for pharmaceutical facility

    The pharmaceutical facility has a variety of manufacturing and production capabilities supported by microbiology, chemistry and R&D laboratories. Clearly understanding what it will take to achieve their vision as an industry leader, they are vigilant in its investment in new R&D, the expansion of its current injectables and inhalation lines, and making production improvements to its delivery systems.
  • Leading Bottled Water Plant Chooses Evoqua’s UV Disinfection Solution

    Water quality is important not only in terms of safety but also has significant impact on the taste, product integrity, cleaning, and sanitation in the beverage industry. The water that has been contaminated with varieties of pathogenic bacteria can pose a threat not only to human and animal health, but also effects the product down time like the water used in the boilers and cooling towers...