-
Italian Utility Improves System Reliability and Saves Water, Money and Energy by Locating Water Loss on a Submarine Pipeline
According to Utilitalia, 38 percent of water is lost on average from the country’s distribution networks. By reducing these losses, the country’s utilities can achieve a more sustainable water supply, lower energy demand, and better financial stewardship.
-
The power of data using MAS 801
O.Y Water’s employees are consistently participating in Xylem’s professional trainings and for three decacdes, they are the people who are recognized with the FLYGT brand in Israel.
-
Xylem’s Jabsco brand and the Global Ecology Group create sustainable disinfection solutions for the COVID-19 pandemic
In response to the COVID-19 pandemic, Global Ecology Group (GEG) developed a fogging system to support the delivery of ECAS solutions in benign disinfection applications. GEG’s Founder and CEO, Owen J. Morgan, has been developing ECAS since the early 1990’s but enlisted Xylem’s help to create amore accessible, portable ECAS fogging system for everyday spaces such as offices and vehicles.
-
Xylem’s Flygt N 3312 electric pump provides non-clog sewer bypass solution
The city of Columbia, Tennessee, experienced a major pump failure in the spring of 2020 that led to sewage overflows, spurring them to engage Xylem Rental Solutions for an emergency pump rental. Xylem engineered a custom temporary bypass system with Flygt electric submersible pump.
-
Alberta Utility Averts Potential Catastrophic Holiday Failure with Proactive Pipeline Management Approach
To ensure safe and reliable water service for its customers, EPCOR partnered with Pure Technologies, a Xylem brand to complete a high-resolution condition assessment. The team inspected a 9.4-kilometer (5.8-mi) section of the critical Northside Pipeline for leaks and pipe wall deterioration.
-
Temporary fire protection systems keeps long-term care hospital facility online
Retrofitting or upgrading the fire protection system of an existing facility is not uncommon, necessitating a temporary fire protection solution that integrates with the existing pumping system to ensure continuity and compliance.
-
Beyond Failure Prevention - The Benefits of Pipeline Monitoring for Large-Diameter PCCP Assets
By implementing a proactive management program, utilities can virtually eliminate the risk of failure within their PCCP inventory. Even utilities that have not experienced a large-diameter PCCP failure, can realize significant capital program savings by managing these assets in place of replacement.
-
Beyond the Wires
While evaluating wire breaks are an important part of PCCP management, it is important to acknowledge additional factors beyond wire breaks. By acknowledging additional condition factors, limitations of wire break assessment, and considering other rehabilitation approaches, there may be a more sustainable PCCP management approach.
-
What's in the Numbers?
The most effective strategy to safely manage a force main inventory is to implement a risk based approach for any data collection, inspection, condition assessment, and management techniques. Using asset risk to guide the management strategies, an owner/operator can ensure they are implementing the right approach, at the right time, with the lowest financial impact.
-
Proactive pipeline management saves utility over $1M
Discover how the Lake Huron Primary Water Supply System leveraged Xylem’s advanced monitoring and inspection technologies and engineering analyses to identify urgent repair needs and plan future maintenance and capital projects. Learn how this approach helped the utility improve reliability, save money, and extend the life of critical infrastructure.
-
Advanced analytic solutions used to implement state-wide monitoring program to improve asset reliability and resiliency
Air Selangor is a large water distribution company owned by the Malaysian state of Selangor. The public utility serves a population of 8.4 million residents and manages over 6200 kilometers of trunk mains, ranging from 300mm up to 2200mm, with much of the pipelines located in remote areas of the state.
-
-
Xylem designed an engineered-to-order water injection pumping solution for a nuclear power plant
Safety upgrades imposed by the United States Nuclear Regulatory Commission (NRC) several years ago required nuclear power plants across the United States to review operations and enhance safety protocols. As a part of this process, a nuclear power plant located in the northeast of the U.S. sought an emergency back-up solution to inject cooling water into the plant reactor in the event that all other means of cooling failed.
-
A Xylem dewatering solution is going strong at an Alliance coal mine six years after installation
Alliance Resource Partners, L.P. faced a two-pronged water challenge at one of its many underground mines. At the South Mine of the company’s Gibson County Coal in Indiana, solid-laden water needed to be pumped out of the mine, and a dewatering system needed to be installed in an area with limited space. Multiple pumps had to fit into a mine void less than eight feet high with a narrow, 20-foot entry span.
-
Xylem installs a flexible, high-efficiency surface water pumping system
Delta Sand & Gravel Co., located in Eugene, Oregon, has been providing quality aggregate materials, service and expertise for almost nine decades. The company offers a full line of aggregate products for year-round, all-weather construction and demolition landfill. Xylem has partnered with Delta Sand & Gravel since 2013, to provide holistic water management solutions.
-
Xylem Delivers Actionable Data Within a Tight Time Frame to Enhance the Safety and Resilience of a Nuclear Power Plant
A condition assessment helps to understand the state of the prestressing wire which provides the pipe’s strength. PCCP manufactured during the 1970s is prone to low ductility in the wire and susceptibility to hydrogen embrittlement, both of which increase the risk of failure. Worn PCCP can rupture with no warning, potentially shutting down the entire facility.
-
Pipeline Inspection of Critical 20-year-old Mine Discharge Water Pipelines in Sensitive Area
In the U.S., mines operate under strict Environmental Protection Agency (EPA) regulations; as such, pipelines must be carefully monitored and maintained.
-
Integrated Water Management System Supports 15% Increase in Production at Aggregates Processing Plant
One of the largest U.S. producers of construction aggregates decided to relocate their processing plant to facilitate increased production capacity. However, the new location was further away from the plant’s water supply.
-
Xylem’s Holistic Solution of Mixers and Pumps Supports Efficient Mine Slime Transport – From Sump to Surface Disposal
One customer, operating a hard rock nickel mine in Ontario, needed an efficient and reliable solution to transport its mine slime from an underground sump back to the surface while ensuring continuity in production and minimizing downtime.
-
Remote Pumping Solution helps Mine Operators Reach New Depths in Harsh Environment
A customer in Perú needed to drain water as its large open-pit mine operation reached as deep as 1,200 ft (365 m) below the surface. The discovery of more copper in the mine, and an expected excess of water during rainy summer months also prompted the company to act. They sought a remote solution for monitoring and controlling their pumping system, particularly as routing electrical power became more difficult the deeper they dug....
-
Xylem partners with Hometown H2O to install water well for retired Oregon couple
For 34 years, Steve and Lana Gleason made due without a traditional residential water system. The couple, who live in the rural logging community of Jewell, Oregon, pumped water for washing from a nearby river and made 40-mile round trips from their home to haul drinking water from a spring.
-
Three thousand assets from the Municipality of Ede in XDM
The Municipality of Ede comprises ten residential nuclei located in one of the most beautiful, wooded parts of the Netherlands. A total of more than two thousand pumping stations have to be managed and maintained there, for which a maintenance management program is used.
-
Xylem’s Flygt Concertor Saves $20,000 Per Year in Maintenance Costs at Coal Fired Power Plant
Operators of one of the largest coal fired power plants in the US based in Michigan, were looking for an efficient, robust and reliable pumping solution to move sludge water from each of the plant’s four sumps.
-
Cleaning of disc diffusers makes Prochamp’s wastewater treatment greener
Soon after starting this biological treatment method, the membrane disc diffusers were found to be clogged with scale particles. However, this problem was satisfactorily solved by the Xylem’s mobile cleaning service: the Diffuser Liquid Cleaning Service.