-
-
-
The Annual Hydrograph of the Ruki River
The group selected the Ruki River, a large centrally-located tributary to the Congo. The Ruki represents only 5% of the total Congo Basin by area but is uniquely blanketed by homogenous pristine lowland forest land-cover.
-
Dam Removal in Washington Yields Flow Management Challenge
An ambitious plan to turn back the hands of time by nearly a century on the Elwha River in northwest Washington State is being carefully studied by stakeholders on other river systems where long-standing dams may someday be breached. Dismantling two concrete hydroelectric dams built in the early 20th century requires careful planning, skilled execution, and close attention to the flow of water that will nurture the reemergence of the river’s salmon population.
-
Accoustic Doppler Current Meters
But behind the massive tunnels and the huge catch basins is a system just as staggering – the SMART Project’s nerve system, a network of flood detection equipment and automated management machinery linked by a Supervisory Data Acquisition and Control (SCADA) brain that uses the information it gathers to automatically engage flood management gates and pumps.
-
Continuous Data Keeps Brazilian Ports’ Business Flowing
HidroMares has installed its SISMO systems at seven port complexes around Brazil, from ocean terminals in the south to an inland river port in the Amazon basin. At the heart of each system is a SonTek acoustic Doppler current profiler (ADCP), which provides current velocity and direction data throughout the water column, as well as water level.
-
Sontek (Argonaut) SL Automated Gaging of the Narmada Main Canal - India
India is emerging as a world leader in irrigation schemes, and the 458-km Narmada Main Canal – the largest concrete-lined irrigation canal in the world – stands as a monument to the opportunities and challenges that face water providers.
-
HydroSurveyor Enables Rapid Reservoir Surveys
The ARC-Boat was developed by HR Wallingford and employs SonTek-proprietary Acoustic Doppler Profiler (ADP®) technology. The HydroSurveyor is a highly sophisticated system which includes 5-beam depth sounding, water velocity profiling and navigation capabilities. When mounted in the ARC boat, the HydroSurveyor scans the reservoir as it is guided across the water’s surface. Recorded data is then analyzed by HydroSurveyor software to produce accurate depth measurement in addition to bathymetry maps of the entire water body. With a small amount of post-processing in GIS or 3-D CAD, an accurate water volume can be determined.
-
App Note: Sontek-IQ Shallow Flow Meter Revolutionizes Flow Measurement in the Australian Bush
It’s hard to picture just how flat Australia’s Murray-Darling Basin is, but picture this – tens of thousands of square kilometers braided with slow-flowing rivers and streams with virtually no fall in their channels.
-
-
-
Hydrosurveyor Enables Rapid Indian Railways Bridge Surveys
The HydroSurveyor-M9 system from SonTek, a Xylem brand, is an instrument/technology that Indian Railway has employed to rapidly measure bathymetry data along with velocity data.
-
London Heathrow's network of 120 pumping stations needed a smart, energy efficient solution to address chronic clogging in aircraft toilet wastewater
Xylem’s Flygt Concertor, with integrated intelligence that uses sensor monitoring, self-optimising technology and adaptive hydraulics, was the perfect smart, energy-efficient processing method.
-
Boracay Island replaces chlorination-dechlorination process with UV disinfection
The Philippine government, through the Department of Environment and Natural Resources (DENR), implemented several measures to reform the island. Closing it for 6 months, the government began clean-up and implemented strict regulations for sustainable water and responsible tourism.
-
Scottish Water pledge to make its network as efficient, resilient and cost effective as possible
As part of Scottish Water's asset resilience strategy, it trialled Xylem Concertor, the first wastewater pumping solution with integrated intelligence, at two of its Ayrshire pumping stations: Maple Grove and Cross Dene.
-
Lowara Pumps help support a unique nickel extraction project
The Thakadu Nickel Purification Plant utilises a process called Nickel Crystallization. A crude nickel sulfate stream is pumped to the purification plant, where it is heated and evaporated into a vacuum, forming nickel sulfate crystals for harvesting.
-
Xylem technologies enable customized heating/cooling system for sustainable packaging business in the US
Xylem’s channel partner Anderson Process was tasked with designing a custom system that could efficiently and reliably heat and cool the oil to the desired temperatures. The team custom engineered a skid incorporating an assortment of fluid handling components, including a Goulds Water Technology e-SH pump and two Standard Xchange heat exchangers.
-
City of Richmond reduces CSOs by 180 million gallons annually and avoids $725M in capital costs thanks to decision intelligence
For decades, the City of Richmond’s Department of Public Utilities has been working to reduce combined sewer overflows (CSOs) and improve water quality in the James River. Despite making significant improvements, the City still experiences between one and three billion gallons of annual overflow and is actively working to reach Department of Environmental Quality (DEQ) water quality goals.
-
-
Non-Genuine UV Lamp Replacement Compromises Performance and Water Treatment Reliability
An increasing number of certification bodies, including NWRI and the USEPA’s UVDGM, require the use of original components in UV water disinfection systems to achieve compliance. But certifications and local compliance policies are different in different parts of the world, including the Middle East region.
-
Flygt hydro turbines prove to be smart solution for small-scale hydroelectric power project
Even in coal-dominated Kentucky, renewable energy is getting more attention as federal and state tax incentives add up, and the federal government moves closer to capping carbon dioxide emissions and making coal power more expensive.
-
Continuous monitoring saves money, prevents failures, and improves long-term planning for California Water Authority
The Water Authority was one of the first agencies to take a proactive PCCP management approach. They began an aggressive condition assessment program in 1992. This early program relied primarily on internal visual and sounding inspections.
-
Hometown H2O program gifts East Texas family with clean, running water
Water Well Trust, a nonprofit partner of Xylem and Hometown H2O, is a domestic water program working to bring access to clean and sustainable water to the more than 2 million Americans without it.
-
Aquavar IPC with NEMA 3R enclosure helps make farming operations more efficient and profitable
Pumps are everywhere in agriculture, essential both for irrigation and for heating, ventilation and cooling (HVAC). But water needs change, and irrigation systems don’t always require a constant flow rate or constant pressure. Variable frequency drives (VFDs) are electric controllers that vary the speed of the pump, allowing the pump to respond smoothly and efficiently to fluctuations in demand.