It looks like you are coming from United States, but the current site you have selected to visit is Saudi Arabia. Do you want to change sites?

Yes, please. No. Keep me on the current site.

Installing your pump system step by step

Table of content

The S1-200 is a very easy to install plug and play pump. Follow these steps to install the pump in any waterv source:

1. Install the S-Connect app

Downloading the S-Connect app

2. Connect a hose to the pump

3. Attach a safety rope to the pump

4. Mount the controller

For more information about mounting the controller, please refer to the following link:

Mounting the controller

5. Connect the PV modules

For more information, please refer to an example in the following link:

Connecting two 100 W PV modules in series

6. Connect the motor cable to the controller

7. Connect accessories

Function and use of remote tank switch

Function and use of tank full switch

Function and use of dry run protection

8. Connect the PV Cable to the controller

9. Place the solar modules so that they face the sun

10. Place the pump in water

11. Turn on the controller

How to switch on the S1-200 pump system

12. Use the S-Connect app to manage your pump

Using the S-Connect app with your pump system