iPERL International Customer Stories

Satu Mare, Romania

Meet iPERL™—the data-driven smart water meter that ensures your networks run efficiently and accurately whilst increasing your business intelligence in near-real time.

Does your network run with unique, cutting edge technology that provides industry-leading accurate and near-real-time data?

iPERL™ is a next generation, solid-state water meter with integrated bi-directional communications capabilities ensuring near-real-time control anywhere in your network. The invaluable benefit of having a meter with no moving parts is seen with the flexibility it affords when considering installation locations; trapped air, dirty water and sand do not affect the high-performance of the iPERL at any stage of its service life.

How many other meters use innovative technology that guarantees sustained accurate data reads over their service life? This ensures you have up-to-date business intelligence, enabling optimum operational efficiency across your entire network and a wealth of data allowing you to conserve water, provide accurate billing to customers and to inform them about leaks, fraud or unusual usage patterns. Sounds pretty smart to us…

iPERL’s key features:

  • Low-flow measurement: With a flow measurement down to 1 litre per hour, iPERL helps utilities to reduce undetected leakages due to next-generation sensors embedded in the endpoint. This technology also includes remnant magnetic field technology, which differs from solid-state meters and provides a constant linear working flow range
  • A wealth of data: The endpoint can be programmed to provide highly granular data at 15-second intervals. The embedded innovative communication enables the possibility of obtaining very detailed data from the meters, including the log of up to 2880 data points
    and alarms. The data collected helps water utilities to manage distribution networks more efficiently, to conserve water, to provide accurate billing to customers and to inform them about leaks, fraud or unusual usage patterns
  • Solid-state meter with no moving parts: Unaffected by trapped air, sand or particles within the water, which ensures accurate readings from the beginning until the end of its service life, and subsequently preventing unplanned maintenance costs
  • 15-year service life: There’s no need for meter re-calibration or replacement as the measurement accuracy of the meter is certified for life

Read below to find out how companies around the world have benefited from the industry leading technology Sensus offers.

-----------------------------------------------------------------------------------------

The city of Satu Mare, Romania, installs 30,000 iPERL smart water meters and experiences increased operational efficiency, valuable business intelligence and a reduction in non-revenue water.

Challenge

The city of Satu Mare, Romania, had a water network that was riddled with problems, one of which was a discrepancy between sub-meters and the main meters in a house or apartment building. This was commonly seen when using mechanical meters, resulting in a 20-25% difference in readings from the sub-meters and the main meters. This left the city with the challenge of having to either bill the customer individually or not at all.

Another issue the city suffered was that of meter fraud with consumers turning the meter the wrong way to create a reverse flow. Overall, the city’s levels of sustainability.

Solution

After conducting research into the types of technologies that could help, Satu Mare discovered that the iPERL smart meter was well suited to put an end to inaccurate readings, lack of data and fraud as the meters come fitted with alarms to alert the utility of any tampering.

The city decided to install 30,000 iPERL meters in 7,040 homes and 22,960 in apartment buildings. The devices were rolled out in a very short time frame and set up for walk-by/drive-by readout, which would help increase the utility’s operational efficiency and costs.

Results

The drive-by readings were so efficient that the water utility was able to reduce meter read-out times of 2,500 devices that would usually require 10 people over seven days, to two people over a mere two hours and 30 minutes. With the high-performance meters, they were able to detect an increase in consumption, with peaks over time which lead the utility to investigate and discover a consumer leak.

The city of Satu Mare was pleased with the results that the data from the smart meters provided, as well as the benefits that having a meter reading at a distance provided the employees with. Now the utility can look forward to increasing operational efficiency, accurate data and conserving water.

How can your smart water grid benefit from being connected at every point?

  • Reduce non-revenue water through accurate data
  • Improve operational efficiency and customer service with bi-directional radio communication
  • Performance uninterrupted by installation due to no moving parts
  • Flexible meter reading solutions with either handheld devices or walk-by/drive-by or fixed network options

-----------------------------------------------------------------------------------------

The market town of Dießen, Germany, relies on economical, ecological and future-proof iPERL metering solution from Sensus to install regulation-compliant lead-free meters.

Challenge

Dießen, Germany, needed to future-proof their water meter network after the German Drinking Water Ordinance introduced a stricter threshold for the amount of lead allowed in drinking water. It was changed to a maximum of 10 μg/l which serves to encourage water utilities to modernise their drinking water installations.

Solution

To ensure they comply with the regulations in the future, the town of Dießen has made a conscious decision to install lead-free meters like the iPERL. Michael Deininger, the Technical Director of the Dießen water utility, said: “When choosing our new water meters, it was important for the materials to comply with the permissible values, but also ensure our decision is future-proof.”

The iPERL smart water meter consists of composite materials and is 100% lead-free, so water utilities can confidently rely on iPERL to ensure they are on the safe side even if threshold values for lead are lowered or if environmental safety regulations become stricter.

Result

“The exceptionally long service life was yet another reason for us to choose iPERL”, Deininger explains. “Longer deployment cycles mean we can reduce the costs which arise from exchanging meters and we can then invest the money this saves in additional state-of-the-art, durable meters.” The added features the meter brings like contactless data reads and magnetic-inductive flow measurements ensure reliable meter performance throughout iPERL’s long and unrivaled service life. Also, process steps such as venting or flushing meters can be dispensed with which eliminates the risk of faulty installation or implementation. These are important economic advantages and have a positive effect on a utility’s operations.

Did you know?

  • The iPERL has the Widest working-flow range on the market
  • It can withstand temperatures as low as -20°C
  • The iPERL is made from sustainable endpoint material
  • It has a unique power supply design
  • Only the water in the supply is measured so air does not add to the volume recorded

-----------------------------------------------------------------------------------------

The Bad König municipal utility company in Germany installed 2,700 iPERL smart water meters in 2014, increasing their operational efficiency and reducing water loss.

Challenge

The Bad König municipal utility company wanted to be the pioneering water utility in Germany moving away from traditional mechanical meters to smart meters, in order to function in a sustainable manner and increase operational efficiency.

They investigated several suppliers to see who would be able to supply them with the best solution: “When we went to see the Sensus plant in Ludwigshafen with its highly sophisticated test labs, we were totally convinced by the manufacturer’s expertise,” says Markus Kunkelmann, Head of Technical Operations at Bad König’s municipal utilities.

Solution

They began their pioneering project by installing quality metrology with its low start-up threshold of just one litre per hour and noted: “We were really surprised with the difference iPERL makes in comparison to the more traditional impeller wheels and oscillating piston meters,” says Kunkelmann. The technical support provided by Sensus played a key role in achieving such positive results in Bad König.

Result

Following the installation of 2,700 meters, the time of data transfer was reduced from a staggering 960 hours to 51. Not to mention, one million litres of drinking water saved in the first year following the installation of iPERL meters.

The economic benefits of iPERL also become apparent when reading the consumption data. Before they deployed iPERL, four members of staff needed 30 days to send the water consumption details to the accounts department. However, with walk-by readings, the complete supply network can be read and all the data sent to the billing department without any errors in just over two days. They have optimised their operating results, reduced water loss, improved their customer relationships and are helping to protect the environment as well.

If you can’t measure, you can’t manage

The data captured by a Sensus iPERL smart water meter, which is often used in conjunction with the FlexNet communications platform, provides your business with the accurate information to identify and help manage network issues proactively and efficiently. It also helps you address regulatory and environmental challenges whilst improving customer service, security of supply and operational efficiencies.

DOWNLOAD PDF