It looks like you are coming from United States, but the current site you have selected to visit is Saudi Arabia. Do you want to change sites?

Yes, please. No. Keep me on the current site.

Remote Inspection Kit Configuration

Before the device is added to Secure Connect, the gateway must be turned on. For further instructions on the hardware connections, download the Remote Inspection Kit Installation Guide. The gateway is fully functional approximately seven minutes after it has been turned on. When the gateway is ready, then it has the following appearance:

LED indicator  Appearance
Power Blue and stable
Cellular connectiviy Green and blinking slowly
User 3 Orange with quick double pulses

 

  1. When the device is added to Secure Connect, then fill in the required fields:
Parameter Values Description
Device type Remote Inspection Kit The device type
Name - A name for the device
MAC address   The MAC address on the back of the gateway
Installed PAN units 0-3 The number of installed PAN units in the station
Pumps: Pump data Enabled or Disabled Enabled: Secure Connect shows the pump data.
Disabled: Secure Connect does not show any pump data
Level sensor Enabled or Disabled Enabled: Secure Connect shows the level data from a sensor that is connected to the gateway.
Disabled: Secure Connect does not show any level data from a sensor that is connected to the gateway.
Level sensor: Model – 4-20mA
– LTU 403
The model of the level sensor
Level sensor: Unit – m
– ft
The unit of measurement
Level sensor: Range min - The minimum value of the level sensor
Level sensor: Range max - The maximum value of the level sensor
Camera Enabled or Disabled Enabled: A camera is included.
Disabled: No camera is included.
Camera: Serial number - The serial number on the back of the camera
The letters must be capitalized.
Camera: Name - A name for the camera
Camera: Position – Aimed at the well
– Unspecified
The position that the camera has in the station

 

  1. Set a threshold for pump running status:
    1. Go to Devices.
    2. Select Remote Inspection Kit.
    3. Go to the tab Data point thresholds.
    4. For each pump, set a power threshold.
      The threshold means that the pump is running. It is recommended to set the value to 10% of the rated power of the pump.
    5. Click Save.
  2. Turn on the camera stream:
    1. Go to Camera.
    2. Next to Camera off, click the switch.
    3. Configure the camera stream under Devices > Camera > Configure device