-
Italian Utility Improves System Reliability and Saves Water, Money and Energy by Locating Water Loss on a Submarine Pipeline
According to Utilitalia, 38 percent of water is lost on average from the country’s distribution networks. By reducing these losses, the country’s utilities can achieve a more sustainable water supply, lower energy demand, and better financial stewardship.
-
Inspection Insights Enable Utility to Extend the Life of a Critical Raw Water Main Reducing Costs
Scottish Water has a 25-year strategic plan for renewing infrastructure to provide high-quality water services that benefit people and the planet. Aging infrastructure is one of the utility’s primary challenges, with many pipelines built over 50 years ago and some well over 100 years old.
-
-
Smartball® Technology Used To Successfully Identify Leaks On Vacuum-Insulated Hot Water Pipeline
Fortum’s core business in Poland is high-efficiency combined heat and power production and heat distribution. The company aims to develop sustainable solutions for cleaner cities, meeting the needs of local communities.
-
Utility Justifies an Increase in Their Capital Spending Budget with Advanced Risk Analysis
Over approximately five years, Aurora Water observed a notable increase in water main breaks. With limited resources to renew aging infrastructure, the utility’s pipeline replacement program was struggling to keep pace.
-
Beyond Failure Prevention - The Benefits of Pipeline Monitoring for Large-Diameter PCCP Assets
By implementing a proactive management program, utilities can virtually eliminate the risk of failure within their PCCP inventory. Even utilities that have not experienced a large-diameter PCCP failure, can realize significant capital program savings by managing these assets in place of replacement.
-
Beyond the Wires
While evaluating wire breaks are an important part of PCCP management, it is important to acknowledge additional factors beyond wire breaks. By acknowledging additional condition factors, limitations of wire break assessment, and considering other rehabilitation approaches, there may be a more sustainable PCCP management approach.
-
City of Mesa pinpoints critical leak, avoiding costly delays
Discover how the City of Mesa, Arizona, used Xylem's SmartBall® technology to pinpoint a hard-to-find pipeline leak, safeguarding infrastructure and avoiding costly delays to a transportation project. -
-
-
Continuous monitoring saves money, prevents failures, and improves long-term planning for California Water Authority
The Water Authority was one of the first agencies to take a proactive PCCP management approach. They began an aggressive condition assessment program in 1992. This early program relied primarily on internal visual and sounding inspections.
-
Flower Mound, Texas Prioritizes Repairs, Prevents Failures, and Reduces Risk with Engineering Assessment
The assessment was urgent, as Flower Mound planned to widen a major road next to the main and wanted reliable information on the condition of that particular pipeline before the road was built. Any necessary repairs or replacement needed to be completed prior to construction to avoid significant disruption and additional expense.
-
Implementing a proactive approach to force main asset management
New standards of best practice for force main management involve a variety of methods and technologies to provide data and information with which to make decisions. Utilities can now often perform a detailed condition assessment while the force main remains in service.
-
-
Municipality uses inline leak detection technology to gather actionable data, avoid costly failures, and update alignment of wastewater pressure main
In recent years, the condition assessment of wastewater mains has become heavily regulated and required by law.
-
Nordic City Takes Proactive Approach to Reduce NRW While Gaining Valuable Condition Assessment Data on Critical Water Mains, Avoiding Costly Failures
As part of a pre-emptive program to address non-revenue water loss and understand the condition of their pipes, Gothenburg wanted to conduct a condition assessment and leak detection survey on a series of large diameter transmission mains. The three pipelines were built in the 1960s and made of cement and steel, ranging in size from 1000 mm to 1200 mm.
-
Pipeline Inspection of Critical 20-year-old Mine Discharge Water Pipelines in Sensitive Area
In the U.S., mines operate under strict Environmental Protection Agency (EPA) regulations; as such, pipelines must be carefully monitored and maintained.
-
Preventing Main Breaks With Advanced Inspection Technologies That Identify Stray Currents, Corrosive Soils, And Wall Loss
When the utility identified the main for priority inspection, they welcomed the strategy of combining a SmartBall leak detection inspection with a pilot run of Xylem’s cutting-edge PipeDiver Ultra, an advanced condition assessment platform that analyzes ultrasonic data to deliver actionable insights on the physical integrity of the pipeline.
-
Proactive pipeline management saves utility over $1M
Discover how the Lake Huron Primary Water Supply System leveraged Xylem’s advanced monitoring and inspection technologies and engineering analyses to identify urgent repair needs and plan future maintenance and capital projects. Learn how this approach helped the utility improve reliability, save money, and extend the life of critical infrastructure.
-
Safeguarding water supplies with SmartBall
In 2020, real water loss in the town’s network peaked at 27 percent. Leaks were undermining the town’s critical water conservation efforts. Recognizing the urgency of the issue, the town is deploying innovative solutions to combat water loss and ensure a sustainable water supply.
-
Scottish Water deploy SoundPrint® Acoustic Fibre Optic System
Scottish Water partnered with WRc and Xylem to inspect the Blairlinnans water main using SmartBall® acoustic leak detection platform and PipeDiver™ electromagnetic condition assessment technology in combination with detailed engineering analysis.
-
-
What's in the Numbers?
The most effective strategy to safely manage a force main inventory is to implement a risk based approach for any data collection, inspection, condition assessment, and management techniques. Using asset risk to guide the management strategies, an owner/operator can ensure they are implementing the right approach, at the right time, with the lowest financial impact.
-
Why high performing utilities choose strategic valve rehabilitation
Around the world, critical valves are in poor repair, or even inoperable. When critical valves fail, managers have effectively lost control of their system, increasing vulnerability to water main breaks or any other system hazard. Once valves have failed, utilities have traditionally sought to replace them, often at great cost, both in terms of time and expense.