-
-
-
-
-
-
-
-
-
-
-
Lowara pumps drive livestock operations
In a major breeding farm from Bergamo, Italy, Rota Guido Srl has installed two reverse osmosis (RO) and ultrafiltration plants that, coupled with a biogas plant ensure local livestock operations are efficient, sanitary and environmentally responsible.
-
-
-
-
-
Leather processing hots up with new Lowara e-SV for high temperature applications
The new e-SV ”Boiler” 180°C can pump water at 170°C for 12 hours continuously without the need for regular external maintenance such as mechanical seal cooling, which is of enormous benefit to the customer.
-
-
-
-
Goulds Water Technology rainwater for today’s high water demand households
In the remote dry Southwest, where water scarcity and escalating demand are daily issues faced by homeowners, third generation Goulds Water Technology professional Kevin Cunningham is finding new uses for Goulds Water Technology variable speed and constant pressure systems.
-
Rodeo’s demands for irrigation and feeding
Agriculture is by far the largest user of water – up to 70% of all fresh water consumption is for irrigation. Water has many other agricultural purposes such as washing stations, misters, or drinking water for livestock. In fact, horses consume up to 15 gallons of water per day.
-
Pumps built to stand the test of time
When Paint/Elk Township Sewage Plant installed a Goulds Water Technology submersible effluent pump in the spring of 1991, they would be set for the next two decades.
-
Xylem helps to save the Sphinx and Giza Pyramids
To solve the groundwater problems, the EAA and United States Agency for International Development created the Pyramids Plateau Groundwater Lowering Project. Hydrotech evaluated the project and selected Xylem’s Goulds Water Technology products as the best solution for the groundwater problem.
-
D&S Pump Supply and Goulds Water Technology keep Quaker Hill Country Club in the green
Over time, the irrigation, pressure boosting and flow control systems at Quaker Hill Country Club became problematic and the grounds crew was only able to water one green or fairway at a time. The possibility of a pump failure forced the staff to monitor the pump continuously while in operation to ensure they shut it down before it ran dry.