It looks like you are coming from United States, but the current site you have selected to visit is Saudi Arabia. Do you want to change sites?
Pumping water in production-oriented applications such as washing, cleaning, food and beverage processing, and large-scale refrigeration, is energy intensive, impacting both resource use and operational expenses. The e-HM pump offers best-in-class efficiency, a broad hydraulic range, and a variety of configuration options that enables users to customize the pump to meet their specific needs, while simultaneously improving performance and reducing carbon dioxide emissions as well as costs.
“Our customers seek total system solutions,” said
The e-HM pump is available in two pump designs and offers a small footprint for compact spaces. It can be custom-configured for a wide range of applications, including chillers, heating, air conditioning and vehicle washing.
For more information about the Goulds Water Technology e-HM series, visit http://www.goulds.com/e-hm.
About Xylem
The name Xylem is derived from classical Greek and is the tissue that transports water in plants, highlighting the engineering efficiency of our water-centric business by linking it with the best water transportation of all -- that which occurs in nature. For more information, please visit us at www.xyleminc.com
Source: Xylem
Xylem Inc.
Jennifer Jacob, +1-914-323-5745
Jennifer.Jacob@xyleminc.com
Xylem