It looks like you are coming from United States, but the current site you have selected to visit is Oman. Do you want to change sites?

Yes, please. No. Keep me on the current site.

Refinery Meets Discharge Requirements For Permit Violations

California refinery completes process to remove contaminants and comply with discharge limits

Challenge

Evoqua Water Technologies was contacted by a large, southern California petroleum refinery for assistance with permit violations for stormwater discharge to a sensitive regional waterway. Identified violations for the discharge included total petroleum hydrocarbon (TPH), phenol, copper, lead, and zinc. The customer faced a five-day deadline to install a treatment system and meet the discharge requirements.

Solution

Evoqua's service-based solution featured removable vessels containing organoclay and carbon for organic treatment, along with multiple stages of ion exchange resins for metals removal. A multiple stage treatment process was necessary to comply with very low discharge limits required at the facility to parts per billion (ppb) levels.

Using Evoqua's wastewater ion exchange service, we were able to rapidly mobilize treatment equipment on-site, while simultaneously analyzing wastewater samples to determine any final adjustments necessary.

Results

Evoqua provided one system comprised of multiple treatment steps to achieve discharge requirements and eliminated further discharge violations. Within the five day requirement, the customer was able to meet the discharge limits and did not experience any additional permit violations.

Evoqua processed the waste carbon media at our RCRA carbon reactivation facility and resin media at the RCRA licensed TSDF located in Roseville, MN. All residuals from the regeneration were further treated and recovered to minimize waste to a landfill. All recyclable waste from the project was recovered as a raw material.