It looks like you are coming from United States, but the current site you have selected to visit is Namibia. Do you want to change site?

Yes, please! No, keep me on the current site

Enable high contrast mode

5 tech-savvy ways to measure flow in places you never thought possible

Original Air Date: Jul 8th, 2014 l Duration: 1:04:51

...and one new instrument to help you get all the data you need!

Welcome to the world of side-looking Doppler technology and the new SonTek-SL 3G! A lot has changed since SonTek introduced the first "sider-looker" back in 1997. With the new SonTek-SL 3G system, scientists, engineers and water monitoring specialists can now collect continuous flow data in places and conditions previously thought unmeasurable. Some of the problems you might be familiar with:

  • Unpredictable, complex flow conditions and frequent changes in water level
  • River/stream/canal cross-section is too narrow
  • Remote monitoring site would be a maintenance nightmare
  • Sedimentation and fouling foes
  • Slow or reversing flow

While frustrating, these problems can be a thing of the past. Product Manager, Janice Landsfeld and Technical Engineer, Brittany Jenner are prepared to talk to you about how the new SonTek-SL 3G can dramatically simplify your flow data collection and profiling efforts. This live, online event will address these five common challenges and offer insight in to the advantages of side-looking profilers as compared to their bottom-mounted or topside counterparts.