It looks like you are coming from United States, but the current site you have selected to visit is Namibia. Do you want to change site?

Yes, please! No, keep me on the current site

Enable high contrast mode

Xylem factory recycles its process water with new treatment plant

Xylem’s manufacturing facility in Emmaboda, Sweden, has a new water treatment plant that recycles the plant’s process water. The plant helps ensure a continuous supply of safe water, even in times of water scarcity, using Xylem’s water reuse technology.

June 27, 2023
Water Reuse

Xylem’s Emmaboda factory is the largest wastewater pump factory in the world, where 1,200 employees produce around 170,000 pumps each year. The factory’s on-site water treatment plant, inaugurated in 2022, can recycle 20 million liters of water each year. The recycled water is used in pump test tanks, for cooling in the foundry, and to dilute cutting fluids in machining processes.
 
The initiative follows years of alarmingly low water levels in southern Sweden, which are expected to become even worse due to climate change. Through its new treatment plant, Xylem will ensure water remains available regardless of external factors.
 
“Following the drought in 2018, our Emmaboda factory was three days away from having to stop production as the city, understandably, needed to prioritize water for the more immediate needs of its population,” says Roger Sandström, Senior Director, Pumps & Circulators, Europe. “Going forward, it is likely that the region will keep facing lower rainwater levels due to climate change. As such, we are excited to launch the Emmaboda treatment plant, which will greatly reduce our usage of regional water supplies.”

A unique water reuse solution combining Xylem technologies

Designed and supplied by Xylem, the treatment plant collects, treats, purifies, and reuses process and stormwater. The plant demonstrates how companies can achieve superior water quality and consistent water flow with Xylem’s water reuse technologies, at low cost and without extensive training. The solution works by leveraging natural surroundings and combining more than 20 Xylem technologies into a compact system.

When used process water leaves the factory, it first passes through a sludge tank to remove heavy particles. It is then collected, along with stormwater, in nearby ponds on the property. As the water sits in the ponds, it undergoes natural settling, as well as biological purification from cultivated herbs. From the ponds, water is pumped to the treatment plant using intelligent, energy-efficient Flygt Concertor pumps.

At the plant, the water passes through five treatment stages – oxidation, flocculation, clarification, sand filtration, and UV disinfection. The incoming water to the plant is analyzed to set appropriate chemical dosing in the first two stages. In the clarification stage, the Leopold Texler lamella clarifier is used to provide a large settling area within a small footprint, removing 98% of impurities. The clarified water then passes through a sand bed to filter out fine particles and contaminants and remove color. Finally, a Wedeco Spektron UV disinfection system provides a microbacterial barrier that eliminates more than 99.99% of all pathogens in just a fraction of a second.
 
Once treated, the water is stored in a clean water reservoir, ready for Lowara variable speed booster sets to deliver it to the factory based on water demand. The treatment process runs automatically while WTW water analyzers, intelligent equipment controls, and a Xylem SCADA system work together to enable real-time, remote monitoring and alerts.

Creating a more water secure future with water reuse

“Water reuse technologies have the potential to create more sustainable water resources for all of us,” says Sandström. “Through this water treatment plant, our aim is not only to reduce our own water footprint but to inspire others to join us in creating a more water secure future. We welcome visitors to view our technology, and to see our facility in action.”
 
Xylem’s Emmaboda plant has additional benefits for the community. For instance, Xylem has designed the facility so that fire trucks can fill their tanks at the Xylem water treatment plant rather than at the municipal plant. The plant can also be used to educate visitors about water treatment, and how different chemical dosing affects the water.
 
Considering the overwhelming stress put on water supplies by growing populations and climate change, heightened efforts are required by businesses and governments to alleviate water scarcity. Through advanced products and technologies, Xylem has enabled customers to reuse over 7 billion cubic meters of water since 2019.