It looks like you are coming from United States, but the current site you have selected to visit is Namibia. Do you want to change site?

Yes, please! No, keep me on the current site

Enable high contrast mode

Beyond the pump: How smart circulators are changing HVAC performance

Choosing a circulator used to be a fairly simple task. Today, it is tied to a much broader set of expectations. Planners and installers are being asked to deliver heating and cooling systems that are efficient, reliable, easy to commission and comfortable for the end user. They also have to do this in a market shaped by high energy prices, tighter regulations and increasingly complex system designs.

So the discussion has shifted. It is no longer just about finding a pump that technically fits the application. More often, the real question is which solution helps professionals achieve the best overall system result while keeping installation and setup manageable.

To look at how these demands are evolving, we spoke with Andras Kovac, Director Product Management for Building Services at Lowara, about what planners and installers are seeing in the field today and how circulator selection affects performance far beyond the pump itself.

Q: What are the biggest challenges planners and installers are facing today?

A: One of the main changes is that HVAC systems have become much more dynamic. With the growth of heat pumps, hybrid systems and variable flow applications, installations are no longer as predictable as they once were. At the same time, the people designing and installing these systems are under pressure to work quickly, avoid errors and still deliver a high level of performance.

So the challenge is not simply to make the system run. It is to make sure it runs efficiently, delivers the right level of comfort and does not create unnecessary work during commissioning or later service visits. That is where many professionals feel the pressure most.

Q: How have customer expectations changed?

A: Customers expect more consistency than before. Whether in residential or commercial buildings, they want comfort, low energy use and quiet operation. They also expect systems to work properly from the start, without the need for repeated manual adjustments.

That has a direct effect on installers and specifiers. Most end users will never think about the circulator itself, but they will notice if the system is noisy, unstable or expensive to run. In that sense, component selection has a very visible impact on the overall customer experience.

Q: What are the most common mistakes when selecting circulators?

A: Oversizing is still one of the most common issues. It often comes from a desire to be cautious, but in practice it can lead to the opposite of what was intended: higher energy consumption, more wear and less efficient operation.

Another issue is that some systems are still designed with a fairly static mindset, even though real HVAC operation is now much more variable. A system may appear correct on paper, but if the circulator is not suited to real operating conditions, performance in everyday use can suffer. The right choice is usually not the biggest option, but the one that matches how the building actually works over time.

Q: So what should professionals focus on instead?

A: It helps to look beyond the initial purchase price and consider the overall effect on the installation. A well-selected circulator can reduce energy use, make commissioning easier and improve long-term reliability.

That broader view is becoming more important across the market. Professionals are increasingly asking not only whether a pump fits, but whether it will help them finish the job more efficiently and deliver strong results over the life of the system. That is often where the real value lies.

Q: Where do residential applications place the greatest pressure on installers?

A: In residential projects, speed and simplicity matter a great deal. Installers are often working under tight time pressure, especially in replacement jobs, and they need products that are straightforward to fit and easy to get running.

This is where the Lowara ecocirc range is especially relevant. Its compact design and simple installation help make replacements quicker and less complicated. For the end user, that also means lower energy consumption and quieter operation from the start.

Q: And where does Lowara ecocirc+ add value?

A: As systems become more variable, automatic adaptation becomes more valuable. Many HVAC installations do not operate under one constant condition, so a pump that can respond to changes in demand reduces the need for manual intervention and helps maintain efficient operation.

That is the role of ecocirc+. It adjusts automatically to changing conditions in the system, which can shorten commissioning time, reduce on-site adjustments and support more stable comfort and lower energy use in day-to-day operation.

Smarter control on site: with the my ecocirc app, the pump can be connected via smartphone for easier setup, adjustment and day-to-day handling.

Q: What about larger commercial systems? What do planners and installers need there most?

A: In commercial buildings, the main issue is often managing complexity while keeping performance under control. These systems may include multiple circuits, changing demand profiles and high expectations around uptime, serviceability and operating cost. When something is not working properly, the consequences are usually more visible and more expensive than in smaller installations.

That is where Lowara ecocirc XL can be considered. It is designed for variable-demand commercial systems and can be integrated into building management systems, helping operators maintain stable performance while keeping energy use under control.

A good example is the Quellenhof Luxury Resort Lazise on Lake Garda, where water management is central to both guest comfort and the site’s sustainability concept. The resort includes a 2,000 m² wellness spa and 68 rooms and suites. To ensure immediate hot water circulation in every room, an ecocirc XL recirculation system was installed using two ecocirc XLplus N 32-120F units. This arrangement keeps water circulating through the backbone of the system and allows hot water to reach the farthest room in 4–5 seconds, while alternating pump operation helps maintain efficiency.

At Quellenhof Luxury Resort Lazise, intelligent water management helps ensure a seamless guest experience while supporting efficient operation.

Q: How important are sustainability and compliance in this decision today?

A: They are now central. Sustainability is no longer treated as an optional extra. In many projects, it is already a practical requirement, and that influences product selection from the start.

Lowara supports these needs in several ways. High-efficiency circulators help reduce operational energy consumption, which is typically the largest part of a product’s environmental impact. We also provide Environmental Product Declarations (EPDs), which give third-party verified information on environmental impact across the product lifecycle. Because these declarations follow Product Category Rules (PCRs), they offer a standardized basis for comparison and can support building-level life cycle assessments as well as certification work such as LEED or BREEAM.

For planners, consultants and end users, that means better transparency and greater confidence that the selected solution supports both current requirements and future expectations.

Q: From the installer’s perspective, what difference does the right solution make on site?

A: Usually, the benefits are very practical. Installers value products that are intuitive, dependable and less likely to create problems during setup. When that is the case, jobs are completed faster, there are fewer errors and the handover to the customer tends to go more smoothly.

Ultimately, that is what matters in day-to-day work. The right solution reduces friction on site and gives installers more confidence that the system will perform as expected once they leave.

Q: Looking ahead, what trends will shape the future of HVAC pumping?

A: HVAC systems will continue to become more interconnected, more variable and more strongly focused on efficiency. As electrification increases, particularly through the wider use of heat pumps, pumps will need to respond to a broader range of operating conditions.

That means circulators will play a more active role in system performance than they did in the past. For planners and installers, the implication is clear: the best choice is not just the one that meets the technical requirement, but the one that makes the whole system easier to install, easier to commission and more efficient over the long term. In that sense, selecting the right circulator is not only a technical decision. It is a practical way to improve outcomes for both professionals and their customers.