It looks like you are coming from United States, but the current site you have selected to visit is Malaysia. Do you want to change site?

Yes, please! No, keep me on the current site

Enable high contrast mode

The pump does not start or delivers too little water

If your pump does not start, or delivers less water than expected, please check the following:

Solar Module

  • Check whether all plugs are connected correctly
  • Check whether there is enough irradiation
  • Check whether the PV modules are dirty, shaded or not facing towards the sun
  • Check whether the modules are connected in a correct way, check the input voltage of the controller
  • Check whether the connected solar modules have enough power/voltage

Controller / Wiring

  • The plugs are wet or have not been inserted properly
  • The controller is too hot and needs to cool down

Pump / Hose

  • Is the pump submersed in the water? Check the water level (dry running)
  • The pump is clogged with mud or sand
  • The hose or pipe is blocked, twisted or kniked
  • The water temperature is too high, the pump will stop or not start → check the temperature class of your pump
  • The water temperature is too low → the flow is reduced
  • The pump was exposed to the sun and is too hot
  • The lift is higher than the head range of the pump