-
Immokalee Water & Sewer District: deployment of a comprehensive water management solution
The Immokalee Water and Sewer District was set up in 1978 to provide affordable, reliable water and sewer services to Immokalee, an unincorporated area of Collier County, Florida. The district operates and maintains the water and sewer plants and systems as an Independent Special District of the State of Florida, serving more than 24,000 year-round residents.
-
Manchester City: Efficient rainwater capture and reuse through data and analytics
Manchester City FC is using smart technology and rainwater reuse to reduce potable water use across its Etihad Campus. With help from Xylem’s data-driven platform, the club aims to optimize irrigation and achieve full stormwater reuse by 2026.
-
Orekan (Navarre Regional Government): early warning system to reduce flood risk
The Autonomous Region of Navarre, located in northern Spain, has a surface area of over 10,000 km² and a population of approximately 680,000, concentrated mainly in the Pamplona metropolitan area. It has a highly complex hydrological system, as it is divided between the Ebro River basin, which covers approximately 90% of the region, and the Cantabrian basin, characterized by short, fast-responding basins. -
Metro Water Services: deploying a digital twin to manage drinking water distribution in real time
Nashville’s city government has a deep-rooted history in the water industry, providing drinking water to its citizens since the early 1800s. Today, Nashville Metro Water Services (MWS), Tennessee, serves more than 191,000 customers in Nashville and surrounding counties.
-
EWE WASSER GmbH: application of a real-time assistance system to reduce aeration energy usage and minimize operational expenses
Xylem Vue has helped to reduce Cuxhaven’s WWTP aeration energy requirements by over 26% and meet its effluent quality requirements.
-
Mimizan: reducing inflow and infiltration through centralized data collection and analysis
The Mimizan Federation of Municipalities is implementing the Xylem Vue platform to reduce inflow and infiltration by improving infrastructure monitoring. -
ARA Pustertal AG: reducing aeration energy consumption by 10% in a WWTP thanks to a digital twin
ARA Pustertal AG operates the Innichen-Sexten wastewater treatment plant (WWTP) in the South Tyrol area of Italy. The plant, which has a capacity for 36,000 inhabitants, uses a conventional activated sludge process, with pre-denitrification and biological phosphorus removal.
-
Grand Rapids, Michigan saves one billion dollars as real-time decision support system solves infiltration and inflow problem
After nearly 25 years, Grand Rapids finished retrofitting its combined sewer overflow system to a separate sanitary and stormwater system, completing its long-term control plan (LTCP) in 2015. But now, the City needed to get a better understanding of the infiltration and inflow into these newly separated sanitary sewers to ensure compliance with a mandate from the Michigan Department of Environmental Quality (DEQ).
-
Severn Trent Water: digital twin to optimise energy and emissions in WWTPs
The implementation of a digital twin at the Strongford treatment works has enabled Severn Trent Water to visualise plant performance in near-real time. -
Spain: Digital transformation of utility processes and infrastructure
To expand digital transformation initiatives beyond the city of Valencia, and effectively manage up to 400 different services across a widely dispersed geographical area. Due to the nature of the project and the stakeholders involved, Global Omnium needed to integrate the systems, sensors, and communication protocols which were already installed across the various infrastructures it managed.
-
Stadtentwässerung Celle: Wastewater treatment plant process optimization through artificial neural networks
Celle cuts energy consumption by 22% and chemical use by 56% using Xylem Vue WWTP optimization technology, saving tens of thousands of euros annually. -
Tuas Power Singapore identifies and eliminates harmful transients to improve system reliability and prolong the effective life of infrastructure assets
The power utility supplies high grade water for their own internal processes as well other industrial customers. Tuas Power was experiencing leaks within their distribution network, which were unexpected because these pipelines were less than five years old, made of steel, and laid above ground.
-
Valencia: Digital twin to save 1 billion+ gallons of water annually
Provide integrated, in-depth, real-time knowledge on system, plant, and asset performance which would allow Global Omnium to more efficiently operate and manage the complex water network in Valencia, Spain and the surrounding metropolitan area.
-
ALJARAFESA: Advanced water cycle asset and work order management
Discover how ALJARAFESA modernized water cycle operations with a unified digital platform that connects asset management, maintenance, and leak detection to improve efficiency, responsiveness, and service delivery. -
ApaVital S.A.: Reduction of daily water losses by over 800 m³
ApaVital deploys Xylem Vue to reduce daily water losses by over 800 cubic meters, achieving compliance with EU regulations. -
Digital twin technology helps city reduce combined sewer overflow volume by 247 million gallons, saving $38 million in capital project work
In 2002, the EPA entered into a federal consent decree with MSD, mandating the elimination of sanitary sewer overflows and significant mitigation of combined sewer overflows into receiving waterways. Engineers estimated the cost to mitigate the sewer overflows at $3.1 billion, an unacceptable capital expense to pass along to MSD’s customers.
-
EMASESA: Data lake design and deployment to increase water and energy efficiency
EMASESA (Empresa de Abastecimiento y Saneamiento de Aguas de Sevilla S.A.) is responsible for water cycle management in the Spanish city of Seville and its metropolitan area. The utility supplies approximately 100 hm3 of drinking water to 1.4 million residents in 12 municipalities every year, as well as distributing raw water to 31 municipalities, serving a total area of 1,220 km2. It manages a 4,000 km network, six water reservoirs, 35 pumping stations...
-
Giahsa: Supervision and control of the sanitation network
Improve control, responsiveness, and efficiency of facilities and processes by providing real-time network status information and analyzing historical network and asset data. Increase resource management effectiveness and efficiency to provide customers with the highest level of service at the lowest possible cost.
-
Gruppo CAP: intelligent water network management through advanced analytics and predictive asset planning
Gruppo CAP deployed Xylem Vue's AI-driven platform to optimize its 6,500 km water network, reducing water losses and improving asset management. -
Hong Kong: development of digital twin pilot for trunk mains water systems in selected areas of New Territories East Region
This project aims to build and calibrate a hydraulic model for trunk mains water systems in selected areas of New Territories East Region and deploy the model through Idrica’s Real-Time What-If-Scenarios solution (now called Xylem Vue).
-
Servicios de Agua Drenaje de Monterrey: Reducing non-revenue water and controlling pressure
Regulate and monitor pressures, supervise flow rates, consumption, and non-revenue water (NRW) in different sectors, and bring together system information from various sources including the SADM’s SCADA.
-
Advanced analytic solutions used to implement state-wide monitoring program to improve asset reliability and resiliency
Air Selangor is a large water distribution company owned by the Malaysian state of Selangor. The public utility serves a population of 8.4 million residents and manages over 6200 kilometers of trunk mains, ranging from 300mm up to 2200mm, with much of the pipelines located in remote areas of the state.
-
Buffalo Sewer Authority: wet weather operational optimization and real-time control system
As the level of national awareness for the need to protect our nation’s water resources continued to grow, federal and state regulators pursued a consent decree in 2006 requiring enhancements to Buffalo’s collection system.
-
CHE enhances flood prevention and management in the Ebro river basin
Xylem Vue is helping the Confederación Hidrográfica del Ebro (CHE) reduce flood damage and implement an EWS for stakeholders managing disaster situations in the basin. CHE is the water authority that manages, regulates and maintains the Ebro river basin, which covers a surface area of around 85,000 km2 and takes in 347 large rivers in northeastern Spain.