It looks like you are coming from United States, but the current site you have selected to visit is Montenegro. Do you want to change site?

Yes, please! No, keep me on the current site

Enable high contrast mode

Smith-Blair Dismantling Joint Used In The Panama Canal

Smith-Blair has gotten the opportunity to have many of our products selected as integral parts in the widening of the Panama Canal. This particular product is a restrained dismantling fitting.

Dismantling Joint Used In The Panama Canal.jpg

The picture shows a 12 inch restrained dismantling fitting attached to a 12 inch butterfly valve. The dismantling fitting is epoxy coated with stainless steel hardware and is rated to 250 PSI.

The dismantling fitting will allow for easy removal and re-installation of the butterfly valve when valve maintenance is required. These fittings are part of the new Panamanian subway system pipeline relocation project that involves several thousand feet of pipeline.