It looks like you are coming from United States, but the current site you have selected to visit is Moldova. Do you want to change site?

Yes, please! No, keep me on the current site

Case Studies

Case Studies

  • City of Tulare celebrates 25 years of converting waste-to-​energy

    The City of Tulare, located in California’s world renowned San Joaquin Valley, is known for its rich agricultural and dairy industries. Tulare is home to six large-scale cheese and dairy producers. Like many municipalities, the city is challenged to meet industrial requirements at a reasonable cost while maintaining harmonious relationships with the surrounding community.
  • Xylem partners with COPEG to control screwworm re-infestation

    The Commission for the Eradication and Prevention of Screwworm (COPEG), created by a cooperative agreement between the Republic of Panama and the United States of America, safeguards Panama and the rest of the countries in Central and North America from screwworm re-infestation.
  • Cheesemaker saves money and the environment with ADI-BVF® reactor

    Since 1956, Rothenbühler Cheesemakers has been producing delicious cheese using all natural ingredients and 100% Grade-A milk. Formerly known as Middlefield Cheese, the family-owned company is one of the largest Swiss cheese manufacturers in the United States. Its plant in Middlefield, Ohio, USA, produces five Swiss cheese varieties, as well as high-quality whey ingredient products.
  • Confectionery manufacturer eliminates sludge dewatering

    The client makes several types of confectionery products at its facility. Its wastewater was being treated in a dissolved air flotation (DAF) system, followed by a dual-tank sequencing batch reactor (SBR) activated sludge system.
  • Confectionery manufacturer expands its operations with ADI-BVF® reactor

    The confectionery manufacturer, located in Virginia, was faced with having to establish on-site wastewater pretreatment at its facility. A planned expansion and an overloaded publicly owned treatment works (POTW) led local authorities to require wastewater pretreatment in order to meet discharge limits of 250 mg/l for both biochemical oxygen demand (BOD) and total suspended solids (TSS).
  • Confectionery upgrades wastewater treatment system

    An ADI Systems client was equipped with an anaerobic wastewater treatment system that consisted of an equalization tank, three hybrid anaerobic reactors, a degas tower, and a clarifier. This system was not meeting the client’s needs, as it was only removing approximately 60% of the BOD. Sludge settleability and odor issues in the open clarifier also presented a problem.
  • Xylem and the City of Tulare celebrate a quarter century of keeping California clean

    The City of Tulare, USA, located in California’s world renowned San Joaquin Valley, has some of the strictest environmental regulations in the nation to protect the Golden State’s water quality. Noncompliance can be costly—up to $10,000 a day. Tulare is committed to complying with wastewater discharge requirements set forth by the California State Department of Water Resources Board.
  • Xylem helps AB Mauri rise above its wastewater challenge

    AB Mauri, a division of Associated British Foods (ABF), is one of the world’s largest producers and distributors of bakery ingredients such as yeast, spices, and bread and cake mixes. AB Mauri’s holistic approach to baking includes a wide range of chemistry and technology applications in addition to its high-quality end products.
  • Xylem helps Furmano’s create energy from food waste

    Furmano Foods Inc. is the Susquehanna River Valley’s premier grower and producer of beans, tomatoes, and vegetables. Since 1921, the family-owned company has been combining agricultural and manufacturing technology with environmentally friendly farming techniques to produce wholesome canned and pouched foods.
  • Xylem solves Strauss Dairy’s wastewater dilemma

    Strauss Dairy, part of the Health & Wellness segment of Strauss Group Ltd., is Israel’s largest private dairy. The family-run business processes cheese, yogurt, and flavored milk drinks. The BVF reactor provides Strauss Dairy with a highly effective, yet low-maintenance pretreatment system that is resilient to a variety of operating conditions and loads. Effluent COD is less than 750 mg/l, and SS is less than 300 mg/l at design loading.
  • Garelick Farms reduces loading to local sewer with anaerobic solution

    Founded in 1931, Garelick Farms manufactures a wide variety of beverages including milk, flavored milk, cream, orange juice, iced tea, lemonade, and fruit punch. The company, which prides itself on its fresh, delicious dairy products, has grown from its humble beginnings (when two brothers home-delivered bottles of milk) to become part of Dean Foods with over sixteen hundred employees and four large production facilities.
  • Kellogg Company upgrades its Pikeville wastewater facility

    ADI Systems first started providing wastewater treatment solutions to the Kellogg Company Pikeville Plant (formerly Mountaintop Baking) in Kimper, Kentucky, USA, in the late 1990s. In 1999–2000, ADI Systems was awarded a design/build contract to upgrade the wastewater treatment system due to production expansion at the plant. The upgrade included an ADI® hybrid anaerobic reactor followed by an ADI® sequencing batch reactor (SBR).
  • Kraft Foods achieves excellent nutrient removals

    Due to an expansion in potato chip production, the snack food plant required additional wastewater treatment capacity. It needed to be able to meet strict discharge limits for biochemical oxygen demand (BOD), total suspended solids (TSS), ammonia nitrogen (NH3-N), total nitrogen (TN), and total phosphorus (TP) regulations.
  • Leading Texas dairy expands production capacity

    Lone Star Dairy is a leading producer of value-added dairy ingredients derived from locally-sourced milk. While Lone Star Dairy was already enjoying the benefits of low-rate anaerobic digestion, production capacity was driving flows and loads beyond the capacity of their existing system. Upgrades were needed to remain compliant to protect the downstream publicly owned treatment works (POTW).
  • Milton Sewer Authority reduces wastewater strength by 90%

    Settled in 1771 and incorporated into a borough in 1817, Milton is home to approximately 7,000 people in Northumberland County, Pennsylvania, USA. The municipally-owned Milton Regional Sewer Authority (MRSA) serves many residential customers, but a large portion of the MRSA’s wastewater treatment plant's influent comes from the manufacturing facilities of ConAgra Foods, the food giant that produces Chef Boyardee, Healthy Choice, Andy Capp, LaChoy, and Gulden’s Mustard products.
  • Over 20 years of wastewater treatment at Australia’s oldest dairy

    Warrnambool Cheese & Butter (WCB) has been producing dairy products for over 125 years, making it the oldest dairy processor in Australia. It produces a range of high-quality dairy products for domestic and export markets and has won several awards from the Dairy Industry Association of Australia.
  • Richmond Dairies controls odors and protects the environment

    Richmond Dairies operates its production plant seven days a week, with wastewater volumes ranging anywhere from 20-180 m3/d (5,300-45,500 gpd). The company had been treating this wastewater through a dissolved air flotation (DAF) plant and discharging it to the sewer; however, the system was not meeting Richmond Dairies’ treatment needs.
  • Shearer’s Foods treats tough snack food wastewater

    Shearer’s Foods is committed to protecting the environment. It has made operational changes to do more with less—less water, less energy, less waste. Its production facilities are state-of-the-art, featuring modern equipment, processes, and systems. The company expected no less when it came to selecting a wastewater treatment solution.