It looks like you are coming from United States, but the current site you have selected to visit is Saint Lucia. Do you want to change site?

Yes, please! No, keep me on the current site

Emergency Bypass for Sewer Facility Circumvents Natural and Manmade Obstacles

The Rivanna Water & Sewer Authority (RWSA)

Charlottesville, Virginia

When operators at the Rivanna Water & Sewer Authority (RWSA) in Charlottesville, Virginia discovered a compromise in the 54- inch secondary effluent water line at their Moores Creek Advanced Water Resource Recovery Facility, they took immediate action to address the problem. The obvious solution was an emergency bypass, but the facility needed a temporary system that wouldn’t harm the creek or shut down the critical access bridge crossing it.

Download Case study