It looks like you are coming from United States, but the current site you have selected to visit is Lebanon. Do you want to change sites?

Yes, please. No. Keep me on the current site.

Remote Control

Allows a user to control devices installed on a station remotely

The remote control feature allows a user to control devices installed on a station remotely. The user can set a new pump speed, start a pump cleaning cycle, or perform other operations remotely depending on what device is connected. This feature enables a user to control digital I/Os. There are a few sets of operations in the selected devices that can be controlled remotely. See the device list below:

  • APP 411
  • Digital Output
  • EcoTouch
  • FGC 313/323
  • FGC 401/411/421
  • Hydrovar HVL
  • Nexicon (remote mode in HMI)
  • PS 220

The remote control service must be enabled for the customer and also required to be turned on in the station settings. When the service is enabled, Remote Control appears in the side menu that takes the user to a page with all the devices that have remote control operations.

Related FAQs

Many users have had similar questions about Remote Inspection and Remote Control.