It looks like you are coming from United States, but the current site you have selected to visit is Lebanon. Do you want to change sites?

Yes, please. No. Keep me on the current site.

FAQs for Filter Presses

Filter presses from Evoqua separate suspended solids from liquids

This can vary greatly depending on your process and application. It can be anywhere from 10 minutes to 10 hours or more. We can do a test to determine the answer for your specific application. For a quote on testing, we require a completed data form.

This depends on your process. Cloth selection is as much an art as it is a science. Based on our 1,000 years of combined experience and lab testing, we can make an expert recommendation to you. We supply cloths based on criteria you give us and based on sample processing we do in our lab. Should your process change, we recommend that your cloth type be evaluated for suitability.

The following is general information to help you understand cloths and how they work. For detailed questions, call our customer service department at 800.245.3006.

Cloths for non-gasketed plates are hung over the plate, extending from top to bottom, and are held in place by eyelets that fit over the cloth-pins on top of the plates. With the non-gasketed plate, the filter cloth provides the seal between the plates. Leakage will occur during operation even though Evoqua supplies the non-gasketed plate cloths with latex edging. The latex will cut down the wicking action somewhat, but will not eliminate it.

The gasketed plate allows less leakage than the non-gasketed plate due to an O-ring seal around the chamber and filtration ports. The gasketed cloth has a high-density sash cord sewn around the cloth's perimeter that is caulked into a groove on the plate.

The type of cloth used is determined by the type of process or application performed by the filter press, the operating environment, and the performance required by the filtering media (filter cloths).

The filter cloths come in many different materials including polypropylene, polyester, cotton, and other synthetic materials. The cloths are made from monofilament fibers, multifilament fibers, or spun fibers. The smooth surface characteristic of monofilament fibers can help to improve cake release properties. The uniform circumference of monofilaments also enables fabrics to be produced with consistent pore sizes. Multifilament and spun fibers are produced by twisting several smaller diameter monofilament fibers together into a single strand. They are used to produce fabrics that require a very tight weave and fabrics where high flow rates are not critical.

Filter cloths also come in many different styles of fabric weave. ​

Mesh opening or pore size is also an important consideration when selecting the

This is difficult to determine from just looking at your filter cloth. The question assumes you bought your filter press from us, in which case we will have your information on record.

Call us with your serial number at 800-245-3006.

If you did not buy your filter press from us and you have questions about your cloth you should still call the number above, and we can walk you through some steps to help figure out your problem. We can also send slurry samples to our in-house lab to help assess your situation. Call us for a conversation.​

There is no micron rating on filter cloths. They are rated by air permeability.

It depends on your process, but general guidelines are as follows:

  • Up to 5 cu. ft. 1" air operated diaphragm pump
  • 5 to 15 cu. ft. 1½" air operated diaphragm pump
  • 15 to 25 cu. ft. 2" air operated diaphragm pump
  • 25 to 50 cu. ft. 3" air operated diaphragm pump
  • 50 cu. ft. and above multiple pumps

We furnish a full line of feed pumps. Please call our customer service department at 800-245-3006 for your best sizing and price.​​

It depends on your process, but general guidelines are as follows:

  • A 1" pump should have a 5 hp compressor
  • A 1½" pump should have a 10 hp compressor
  • A 2" pump should have a 12-15 hp compressor
  • A 3" pump should have a 20 hp compressor

Changes in chemical and physical treatment may alter the performance of your filter press. We can assist you in optimizing your press performance by performing lab testing. Please contact our customer service department at 800-245-3006.

This usually means it is time to clean your filter cloths.

Possible causes are:

  1. Dirty filter cloths. What to do: clean or replace filter cloths
  2. Malfunctioning (low) feed pump. What to do: clean and adjust as needed
  3. Incorrect treatment or treatment change. What to do: contact customer service at 800-245-3006

It depends on:

  • The amount of opening space left in your press
  • How much clean-out space you want to sacrifice
  • If your press has an expansion piece

You may be able to buy new, longer sidebars if you have a bolt-on style press.

Call customer service at 800-245-3006.

Safely, none.

We can provide you with a back-up plate if you need to reduce the capacity of your press.

Call customer service at 800-245-3006.

This is difficult to determine from just looking at your filter cloth. The question assumes you bought your filter press from us, in which case we will have your information on record.

Call us with your serial number at 800-245-3006.

If you did not buy your filter press from us and you have questions about your cloth you should still call the number above, and we can walk you through some steps to help figure out your problem. We can also send slurry samples to our in-house lab to help assess your situation. Call us for a conversation.​