It looks like you are coming from United States, but the current site you have selected to visit is Lebanon. Do you want to change sites?

Yes, please. No. Keep me on the current site.

Case Studies

Case Studies

  • Xylem and the City of Tulare celebrate a quarter century of keeping California clean

    The City of Tulare, USA, located in California’s world renowned San Joaquin Valley, has some of the strictest environmental regulations in the nation to protect the Golden State’s water quality. Noncompliance can be costly—up to $10,000 a day. Tulare is committed to complying with wastewater discharge requirements set forth by the California State Department of Water Resources Board.
  • Xylem helps AB Mauri rise above its wastewater challenge

    AB Mauri, a division of Associated British Foods (ABF), is one of the world’s largest producers and distributors of bakery ingredients such as yeast, spices, and bread and cake mixes. AB Mauri’s holistic approach to baking includes a wide range of chemistry and technology applications in addition to its high-quality end products.
  • Xylem helps Furmano’s create energy from food waste

    Furmano Foods Inc. is the Susquehanna River Valley’s premier grower and producer of beans, tomatoes, and vegetables. Since 1921, the family-owned company has been combining agricultural and manufacturing technology with environmentally friendly farming techniques to produce wholesome canned and pouched foods.
  • Xylem solves Strauss Dairy’s wastewater dilemma

    Strauss Dairy, part of the Health & Wellness segment of Strauss Group Ltd., is Israel’s largest private dairy. The family-run business processes cheese, yogurt, and flavored milk drinks. The BVF reactor provides Strauss Dairy with a highly effective, yet low-maintenance pretreatment system that is resilient to a variety of operating conditions and loads. Effluent COD is less than 750 mg/l, and SS is less than 300 mg/l at design loading.
  • Garelick Farms reduces loading to local sewer with anaerobic solution

    Founded in 1931, Garelick Farms manufactures a wide variety of beverages including milk, flavored milk, cream, orange juice, iced tea, lemonade, and fruit punch. The company, which prides itself on its fresh, delicious dairy products, has grown from its humble beginnings (when two brothers home-delivered bottles of milk) to become part of Dean Foods with over sixteen hundred employees and four large production facilities.
  • German sugar factory controls cooling circuit disinfection

    Südzucker produces 5.4 million tons of sugar a year. Situated in Obrigheim, located in the Palatinate region, the Offstein Sugar Factory is one of the largest and oldest of nine sugar factories in Germany. Yearly, 1.4 to 1.8 million tons of sugar beets are processed. During the harvesting campaign (September to December), this is about 16,000 tons of beets daily - around the clock. Syrup and sugar are produced from the beets.
  • Kellogg Company upgrades its Pikeville wastewater facility

    ADI Systems first started providing wastewater treatment solutions to the Kellogg Company Pikeville Plant (formerly Mountaintop Baking) in Kimper, Kentucky, USA, in the late 1990s. In 1999–2000, ADI Systems was awarded a design/build contract to upgrade the wastewater treatment system due to production expansion at the plant. The upgrade included an ADI® hybrid anaerobic reactor followed by an ADI® sequencing batch reactor (SBR).
  • Kraft Foods achieves excellent nutrient removals

    Due to an expansion in potato chip production, the snack food plant required additional wastewater treatment capacity. It needed to be able to meet strict discharge limits for biochemical oxygen demand (BOD), total suspended solids (TSS), ammonia nitrogen (NH3-N), total nitrogen (TN), and total phosphorus (TP) regulations.
  • Leading Texas dairy expands production capacity

    Lone Star Dairy is a leading producer of value-added dairy ingredients derived from locally-sourced milk. While Lone Star Dairy was already enjoying the benefits of low-rate anaerobic digestion, production capacity was driving flows and loads beyond the capacity of their existing system. Upgrades were needed to remain compliant to protect the downstream publicly owned treatment works (POTW).
  • Milton Sewer Authority reduces wastewater strength by 90%

    Settled in 1771 and incorporated into a borough in 1817, Milton is home to approximately 7,000 people in Northumberland County, Pennsylvania, USA. The municipally-owned Milton Regional Sewer Authority (MRSA) serves many residential customers, but a large portion of the MRSA’s wastewater treatment plant's influent comes from the manufacturing facilities of ConAgra Foods, the food giant that produces Chef Boyardee, Healthy Choice, Andy Capp, LaChoy, and Gulden’s Mustard products.
  • Odor and heat contained with modular and biogas covers

    A major American frozen food manufacturer with worldwide distribution required a cover solution for its wastewater treatment system that would reliably contain odors and retain heat. Xylem designed, fabricated, and installed a large biogas collection cover​ for the frozen food manufacturer’s on-site anaerobic digester.
  • Over 20 years of wastewater treatment at Australia’s oldest dairy

    Warrnambool Cheese & Butter (WCB) has been producing dairy products for over 125 years, making it the oldest dairy processor in Australia. It produces a range of high-quality dairy products for domestic and export markets and has won several awards from the Dairy Industry Association of Australia.
  • Quality begins with water at a startup craft brewery

    Brewing high-quality craft beer is a challenge in any part of the country. In Texas, where water quality can vary as the climate whipsaws from drought to flood and back again, it can be especially challenging. Because with craft brewing, the quality begins with the water.
  • Richmond Dairies controls odors and protects the environment

    Richmond Dairies operates its production plant seven days a week, with wastewater volumes ranging anywhere from 20-180 m3/d (5,300-45,500 gpd). The company had been treating this wastewater through a dissolved air flotation (DAF) plant and discharging it to the sewer; however, the system was not meeting Richmond Dairies’ treatment needs.
  • Shearer’s Foods treats tough snack food wastewater

    Shearer’s Foods is committed to protecting the environment. It has made operational changes to do more with less—less water, less energy, less waste. Its production facilities are state-of-the-art, featuring modern equipment, processes, and systems. The company expected no less when it came to selecting a wastewater treatment solution.
  • Award-winning wastewater treatment project completed at recycle paper mill

    Shanghai Xinlun Paper was upgrading its pulping and paper-making process. As this was taking place, new regulations came into effect that required the mill to invest in secondary wastewater treatment so it could meet stringent effluent limits of 100 mg/l chemical oxygen demand (COD), 30 mg/l biochemical oxygen demand (BOD), and 200 mg/l total suspended solids (TSS).
  • Thai beverage replaces over 80% of its heating requirements

    Based in Bangkok, Thai Beverage Public Company Limited is Thailand's largest and one of Southeast Asia's largest beverage companies. It owns and distributes several significant brands, including Chang beer (the top-selling brand in Thailand), Mangkorn Thong and Sangsom rums.
  • Sugar company finds sweet solution for odor control

    The sugar company produces approximately 4,500,000 cwt. of sugar per year, resulting in high-strength wastewater that creates odors, especially during the company’s peak season in the spring and summer. The company was using a series of basins, such as ponds and ditches, to cool, equalize, settle, and digest the organic wastewater.
  • Stonyfield keeps up with yogurt demand

    Stonyfield is a thriving yogurt business with a modern, sprawling plant in Londonderry, New Hampshire, USA. What began in 1983 as a two-person operation on a small farm has grown over the last three decades to introduce many new products, including yogurt drinks, frozen yogurt, and Greek yogurt.
  • Simplot partners with Xylem on wastewater treatment projects

    The J.R. Simplot Company, commonly referred to as Simplot, is one of the largest privately held food and agribusiness companies. The company is headquartered in Boise, Idaho, USA, but it has operations around the globe, including Portage la Prairie, Manitoba, Canada, and Caldwell, Idaho, USA.