It looks like you are coming from United States, but the current site you have selected to visit is Kuwait. Do you want to change site?

Yes, please! No, keep me on the current site

High Efficiency VSX® Pumps Provide Increased Comfort at High-tech Science Oasis

 

King Abdullah University of Science and Technology (KAUST) near Jeddah, Saudi Arabia, combines several planning and design elements that meet under the theme of sustainability. The University’s new campus was constructed from scratch on a 22-mile (36km) stretch of desert 50 miles (80km) north of Jeddah along the Red Sea. The campus is part of a larger master plan which includes a new town of 10,000 to 12,000 people that surrounds and supports the University.

KAUST was designed to propel the Kingdom into the 21st century with modern teaching facilities and equipment costing US$1.5 billion. The University’s mission is to advance science and technology to new levels by educating tomorrow’s leaders while catalyzing the diversification of the Saudi economy and addressing challenges of regional and global significance.

KAUST under construction

All campus buildings meet the strict ASHRAE 55 Standards for thermal and environmental requirements for human occupancy, guaranteeing that interior temperatures and humidity will remain at comfortable levels. Xylem’s Bell & Gossett brand VSX® pumps help meet the campus’ HVAC needs that result from the extreme climate in the region as well as from some very demanding system challenges.

After meeting and surpassing a long list of application requirements – including a minimum specification for 80% efficiency – Bell & Gossett Series VSX double-suction, split-case pumps were selected for district cooling at the University campus. The requirements also set strict guidelines for Net Positive Suction Head (NPSH), and identified limited space areas that required small pump footprints. VSX pumps were chosen because of their proven vertical split-case (VSC) platform that features vertical suction and discharge flanges that reduce equipment footprint by up to 40% compared to horizontal double-suction and large inline pumps.

A total of 27 large Series VSX VSC model and VSH model pumps were installed throughout the campus. These large pumps have motors ranging from 300 to 1000 HP:

  • Nine VSX-VSC 14x16x22A, 7,500 GPM /130 Ft. with 300Hp, 4160V/60/3, TEFC, 1200 RPM motors
  • Nine VSX-VSC 12x14x22A, 7,500 GPM /380 Ft. with 900Hp, 4160V/60/3, TEAAC, 1800 RPM motors
  • Nine VSX-VSH 16x18x19A, 15,000 GPM /196 Ft. with 1000Hp, 4160V/60/3, TEAAC, 1800 RPM motors

As a result of its revolutionary design, the VSX platform offers many installation options. Using CFD technology, VSX delivers identical performance in any of its three flange configurations. The result: users can maximize piping possibilities and meet a broad hydraulic range for chillers, towers, distributive and general pumping requirements.

VSC VSCS HSC

The three VSX pump models include:

  • VSC – top suction and discharge
  • VSCS – side suction, vertical discharge
  • HSC – side suction and discharge

VSX pumps feature:

  • Hydraulic coverage to meet all design requirements
  • Flows from 500 to 28,000 GPM (114 to 6400 m3/h)
  • Heads from 30 to 530 feet (9 to 161m)
  • Working pressures of 175 and 300 psig (12 and 20 Bar)
  • ANSI flange ratings of 125# and 250# – Temperature range from 0°F to 300°F (-17°C to 148°C
  • One-piece unitized seal
  • Speedier installation
  • Alignment-friendly coupling
  • Simplified service
  • Maintenance-free bearings

Coordinating the design and installation of the KAUST HVAC system was a team effort between Xylem and its Bell & Gossett Representative in Saudi Arabia who worked to supply specialized drawings, weekly progress and production schedules, vibration monitoring and compliance with sometimes unfamiliar industrial specifications.

The massive project started in the Fall of 2006, and was finished in just three years. To achieve this ambitious timetable, planning groups accelerated the process with a “Racing the Sun” design in which HVAC professionals from ten offices across multiple time zones contributed to the planning effort during just one 24-hour period.

KAUST’s first class of 400 students was selected from many parts of the world well before the University’s official opening on Sept. 23, 2009. The University’s president, Professor Choon Fong Shih, described the institution as the opportunity of a generation.

“We give our academics the full freedom to pursue exceptional science. We fund them to work together in groups of men and women developing ideas that will make a big impact."
Professor Choon Fong Shih, President, King Abdullah University of Science and Technology

Thanks to Xylem, its Bell & Gossett VSX pumps helped King Abdullah University of Science and Technology meet its requirement for 80% efficiency pumps, as well as solve problems involving limited space and other installation challenges. As a result, KAUST students study in a comfortable environment, and the University is able to achieve its mission to advance science and technology to new levels in the region.