It looks like you are coming from United States, but the current site you have selected to visit is Kyrgyzstan. Do you want to change site?

Yes, please! No, keep me on the current site

Providing revenue to local businesses & healthy meals to those in need

Noland_Triangle_color_winsupply.png              The Chris Long Foundation.png

According to the US Census Bureau, the 2019 poverty average in Charlottesville, VA is 24.5%, which is 14.5% above the national average. The COVID-19 crisis has only exacerbated the need in the community. Through our partner Charlottesville Noland – Winsupply, our grant to The Chris Long Foundation will help the organization provide meals to 1000 people while also supporting locally owned restaurants through its Grub4Good program. By distributing meals through the foundation’s network of nonprofits and city agencies, the program will create a dual benefit of providing revenue to local businesses and providing healthy and safe meals to those who need them.