Search Results
-
Ion exchange services remove groundwater contaminants
California Water Service Company had acquired another water company with approximately 100 connections, in Porterville, California, located in a remote agricultural area of the Central Valley. Their annual well testing had shown levels of nitrate at or near the Maximum Contamination Level (MCL) of 45 ppm and perchlorate was found in the groundwater at levels above the Public Health Goal (PHG) of 10 ppb. A treatment system was needed to remove both these contaminants to ensure quality potable water for the local community.
-
Municipal drinking water treatment
Municipalities are often faced with VOC contamination of their source wells. Chemicals like Vinyl Chloride and Trichloroethylene can leach into aquifers used as source water for municipal wells. When this occurs, in many cases the most cost-effective solution is to treat the water to remove the VOCs using air stripping, which has been established as a Best Available Control Technology BACT for this application.
-
Orange County water district removes PFAS with 30 systems
In February 2020, the California State Water Resources Control Board announced revised drinking water Response Levels for perfluorooctanoic acid (PFOA) and perfluorooctanesulfonic acid (PFOS) in drinking water. The new Response Levels (RLs) were set at 10 parts per trillion (ppt) for PFOA and 40 ppt for PFOS. The previous RL was 70 ppt for a combined total concentration for the two contaminants.
-
Public utility removes arsenic to control underground plume
A public water agency in California contacted Xylem to treat remove arsenic from a groundwater supply. They needed to achieve a 1 ppb effluent level from the treatment system, 90% lower than the current drinking water standard in California. In addition they needed to have the treatment operating within weeks.
-
San Diego plant cuts THM levels in half
The 34 MGD Otay Water Treatment Plant in San Diego, California serves a population of approx. 200,000. The plant receives raw water from two sources - imported water from the Colorado River and runoff from three local reservoirs.
-
SCV Water Agency selects Xylem vessels & media for PFAS removal
Santa Clarita is located about 35 miles north of Los Angeles. The Santa Clarita Valley Water Agency (SCV Water) services nearly 74,000 customers and obtains about 50% of its drinking water through local groundwater aquifers. Positioned behind the William S. Hart community baseball and softball fields three two-vessel systems have been installed to remove PFAS from drinking water.
-
Southern California water utility consults Xylem for disinfection of potable water
Located in Southern California, this water utility uses wells to store water. These same wells are also used for fire protection. which is especially critical during the summer months. The supply covers about 10,000 customer connections with chloraminated water for residual disinfection, with chlorine and ammonia boosting in various locations.
-
Stadtwerke Trier: AI-aided energy optimization for daily energy balancing
Xylem Vue helped Stadtwerke Trier optimize renewable energy use in its drinking water network, achieving 90% self-consumption. -
Tarragona Water Consortium: implementation of an advanced data management solution
CAT implemented the Xylem Vue platform and its Smart Water Engine to solve this problem and boost water and energy efficiency. The Unified Network Management application was implemented to provide a single control center for CAT’s drinking water treatment assets, regardless of their geographical location.
-
Updating London’s drinking water network
A UK water supply company serves a population of approximately 675,000 consisting of homes and businesses in Surrey, Sussex and Kent and is a key part of London’s drinking water network. The largest works in Kent, which takes raw water from a reservoir that is recharged in winter by abstraction from the River Eden. The original works capacity was 35Ml/d and it is currently undergoing a phased uprate.
-
Vermont town of 450 removes PFOA from drinking water well
The source of the contaminated water was located approximately 250 meters away from the municipal well, at a former industrial site. Upon learning of the elevated test results, the state issued a “do not drink” order to the 450 residents served by the municipal water supply until the water source could pass quality testing again.
-
Water plant removes manganese and improves turbidity
This 10 million gallons per day drinking water plant gets its raw water source from a 151,000 acre-feet reservoir situated at an elevation of 5430 ft. The water intake is through a tunnel at a depth of 200 feet. The intake does not have provisions for the withdrawal of water from multiple levels in the reservoir.
-
Xylem removes PFAS from Michigan construction site
"Non-detect" treatment goal met and 21 million gallons of water cleaned in downtown site
-
Tip Sheet
How to Calibrate the DEPOLOX® 700 M Controller
The DEPOLOX® 700 M Controller is applicable for the measurement of chlorine, pH, ORP, temperature and conductivity.
-
Tip Sheet
How to Change Gas Containers on the V10k™ Vacuum Gas Feed System
Learn how to safely change gas containers on the V10k System.
-
Tip Sheet
Maintenance Tips for the OSEC B-Pak Electrolyzer
Regular maintenance of the chlorine membrane electrolysis system is a precondition for the customer to be able to make claims for defects. The below is an extract from the instruction manual.
-
Video
ApaVital: improving utility operations through digital transformation
Learn how this Romanian utility has implemented the Xylem Vue platform to transform its infrastructure and tackle water losses in real time. -
Video
Individual Filter Outlet (IFO) UV Installation
The next generation of UV design that saves space and costs, while increasing operational and environmental efficiency
-
Article
Irrigation in the building sector: why efficiency and automation now start from the heart of the system
For many years, irrigation in the building sector was considered a secondary matter. A necessary system, certainly, but rarely a strategic one. Today, that approach is no longer sustainable. Climate change, water scarcity, rising energy costs and increasing environmental responsibilities are radically transforming the way buildings are designed and managed. -
Blog Page
Ripple Effect: Building a smart water system on Catalonia's coast
How a water utility in Spain is using digital twins and AI to prevent pipeline breaks, anticipate risks, and optimize water management.
-
Blog Page
Ripple Effect: How digital transformation is solving water in Asia
Xylem’s President of China and Asia, Shuping Lu, discusses digital trends across the region and how collaboration is fueling digital transformation.
-
Blog Page
Utilities don't have to choose between modernization and cybersecurity
Utilities can modernize aging infrastructure without increasing cybersecurity risk. Learn how secure-by-design technologies help improve resilience, visibility, and operational performance. -
Blog Page
Why future water leaders matter more than ever
Water utilities face growing workforce challenges as experienced operators retire and digital technologies reshape operations. Learn why investing in future water leaders is critical to resilience, modernization and long-term water security. -
Blog Page
Repair vs. replace: a comparative analysis of large valve management
In the fall of 2017, Grand Rapids contracted with Wachs Water Services to assess and evaluate 20 additional large valves Grand Rapids’ transmission system to pilot the foreign method of maintenance, operation and rehabilitation.