It looks like you are coming from United States, but the current site you have selected to visit is Kyrgyzstan. Do you want to change site?

Yes, please! No, keep me on the current site

EnviroMix’s operational excellence award presented to South Adams, CO



Pictured (left to right): SACWSD staff members Travis Dunphy, Danny Nielsen, and Gary Smith receive the award from Sarah Elger (EnviroMix) and Jeff Rabas (Coombs Hopkins).

In September 2022, EnviroMix presented its Operational Excellence Award to the South Adams County Water and Sanitary District (SACWSD) in Henderson, Colorado.

In 2015, SACWSD upgraded the Williams Monaco WWTP to improve treatment and increase capacity. The new plant design replaced the previous MBBR secondary process with an 8 MGD Integrated Fixed Film Activated Sludge (IFAS) process in an A2O configuration for biological phosphorous removal as well as nitrogen reduction.

Selected by SACWSD and Burns & McDonnell as an integral part of the plant upgrade, BioMix Compressed Gas Mixing was installed in the newly constructed anaerobic and anoxic selectors, and in the existing anoxic selectors, replacing inefficient and maintenance-intensive submersible mixers.

Utilizing a duty and a standby compressor, the BioMix system allows the WWTP to maximize operational reliability. Compared with the previously utilized mechanical mixers, BioMix delivers 50-60% more energy savings and enables the plant to avoid the high maintenance expense.

The attentiveness of the SACWSD staff has been fundamental in the long-term success of this project. EnviroMix is honored to have the opportunity to work with SACWSD.