It looks like you are coming from United States, but the current site you have selected to visit is Kenya. Do you want to change site?

Yes, please! No, keep me on the current site

OPTIMIZE OPERATIONS TO PREVENT PEAK ENERGY CONSUMPTION.

Leveraging data to increase plant efficiency to improve processes and reduce energy is more important than ever. Xylem Treatment System Optimization helps your utility improve treatment plant operations to save energy, minimize chemical inputs and deliver better water and results at optimized cost and effort.

REAL-TIME DECISION SUPPORT.

Integrates directly with your existing SCADA system and creates a real-time digital twin to simulate and optimize complex biological and chemical processes.

2-blu-x-tpo-composite-support-system.jpg

2-blu-x-tpo-composite-lower-cost.jpg

LOWER COST WITHOUT REQUIRING NEW INFRASTRUCTURE.

By utilizing existing infrastructure, you can optimize operations and reduce energy use and operating costs.

A GLASS BOX, NOT A BLACK BOX.

Other digital solutions often operate as “black boxes,” offering little transparency into their processes. Xylem Treatment System Optimization provides direct insight into the functionality of the data collection and integration process.

2-blu-x-tpo-glass-box.jpg

JOIN THE 70+ CLIENTS ACROSS THE GLOBE WHO ARE REALIZING 3X TO 10X MORE ROI.

With Xylem’s Digital Solutions, utility leaders like you are saving millions of dollars while reducing risk, optimizing operations and protecting your environment.

CUXHAVEN, GERMANY SAW A DRASTIC REDUCTION IN UNNECESSARY PLANT FLUCTUATIONS AND PREVENTED SITUATIONAL PEAK ENERGY CONSUMPTION, SAVING ENOUGH ENERGY TO POWER 64 HOMES FOR ONE YEAR.

LET'S SEE THE CUXHAVEN CASE STUDY

LET’S SEE HOW UNLOCKING POWERFUL INSIGHTS DELIVER TRANSFORMATIVE OUTCOMES.

As just one of the digital solutions in our platform of disruptive technologies, Xylem Treatment System Optimization can help your utility improve treatment plant operations while continuing to ensure regulatory compliance and realize savings.

  • Ensure compliance with legal threshold values
  • Reduce chemical consumption
  • Optimize aeration energy consumption rates
  • Increase security from an automatically controlled system
  • Help speed recognition of problems in the plant
  • Result in faster response times to equipment failures
  • Improve understanding of complex plant processes
  • Increase transparency on how performance metrics are achieved
  • Lower concentrations of pollutants in effluent

SENSE, PREDICT AND ACT IN REAL-TIME.

Xylem Treatment System Optimization utilizes a Sense-Predict-Act approach (similar to our Xylem Wastewater Network Optimization solution) that drives continuous improvement by merging real-time data and plant models, augmented with artificial intelligence, to create a real-time decision support system that helps optimize complex sewage treatment systems. When combined with the operational expertise of your plant operators, your utility can optimize energy usage, chemical consumption, and ensure regulatory compliance at less cost.

Xylem Treatment System Optimization also integrates historical and real-time data like SCADA, LIMS and weather into a single system that powers the treatment plant and provides a continuous view of all operations. This data is then used to create a digital twin of your plant that accurately forecasts operating conditions and recommends optimal treatment for current wastewater flow and composition. These powerful tools, combined with automation, give your operators a single source of truth needed to make real-time decisions and optimize the treatment process.

XYLEM TREATMENT SYSTEM OPTIMIZATION ROUTINELY ACHIEVES ENERGY REDUCTIONS BETWEEN 25% AND 30%, EQUATING TO OVER 1 MILLION KWH ANNUALLY. THIS IS IN ADDITION TO REDUCTIONS GAINED FROM EQUIPMENT IMPROVMENTS. 

TAKE THE FIRST STEP TO BETTER ROI.

As a simple, low-investment way to understand your economic opportunity, a Discovery Project is an ideal initial step to taking better control of your treatment plant operations and reducing energy and chemical consumption significantly. It allows us to work together to visualize your entire network, identify challenges and opportunities and begin creating a roadmap to transformational outcomes for your utility and community. Let's see how it works:

blu-x-step-_0001_1-xylem-blux-process-scope.png

 

STEP 1

SCOPE

First, we conduct an initial discovery session to identify your critical system pain point and determine the metrics we’ll use to track our benefits to your plant.

STEP 2

ANALYZE

Next, we’ll use your existing data and analyze the performance of your system to identify opportunities to operate your treatment plant more efficiently and address your pain point at a lower cost.

2-xylem-blux-process-analyze.jpg

7-blu-x-tpo--process-workshop.jpg

STEP 3

WORKSHOP

Finally, we collaborate with you in a workshop where we provide a data-driven presentation and discuss our analysis. The outcome is a high level, prioritized set of recommendations and practical next steps to optimize your system’s operational and efficiency outcomes.

SCHEDULE A DISCOVERY CALL
+

Schedule a Discovery Call Today

Start analyzing your treatment plant to improve operational efficiency and reduce costs.

All fields required.

* Required Field