It looks like you are coming from United States, but the current site you have selected to visit is Jordan. Do you want to change sites?

Yes, please. No. Keep me on the current site.

Efficient handling of wastewater at a harbor

SWEDEN

To prevent pollution by sewage from ships, governments are required to ensure the provision of adequate sewage reception facilities. One of the ports within the Ports of Stockholm were outfitted with a Flygt pump station for the handling of sewage and grey water. To handle the large amount of waste water without clogging a Flygt TOP pump station including N-pumps were installed. Ensuring reliable and efficient pumping in the tough conditions. Download to read the whole story.

Download Case study