It looks like you are coming from United States, but the current site you have selected to visit is Jordan. Do you want to change sites?

Yes, please. No. Keep me on the current site.

Case Studies

Case Studies

  • Xylem selected to supply odour control system for Metro Vancouver

    The South Surrey Interceptor is an extensive piping system that collects and conveys approximately 500 million litres of wastewater daily from municipalities in the eastern area of Metro Vancouver to the Annacis Island Wastewater Treatment Plant located in the City of Delta, British Columbia.
  • Xylem's ArchPro™ odor control covers reduce predicted odor impact

    The Cronulla Wastewater Treatment Plant (WWTP) is one of 30 wastewater treatment and water recycling plants in greater Sydney, the Blue Mountains, and the Illawarra. It is owned and operated by Sydney Water, Australia’s largest water utility. The plant is located on the southern end of the Kurnell Peninsula (about 18 km [11 miles] from the city center), and treats about 54 million liters (14 million gallons) of wastewater a day.
  • The Orbal® system for biological nutrient removal

    Water is precious to the 8000 residents of this town in central Utah, as it is to so many similar places in the arid Intermountain West. Town history attributes Salem City's 19th-century founding to its location as a suitable spot for damming up a local spring to create a pond, which is still the centerpiece of the town.
  • H2S odours eliminated with ZABOCS® system

    A town located in the Western Canadian Rockies prides itself on its natural features that includes a river flowing through the middle of town. The area provides residents and visitors with scenic trails, wildlife habitat, drinking water for the community.
  • Huntertown, IN charts new course with Xylem's Orbal® system

    Just north of Fort Wayne, Indiana, the community of Huntertown boasts the second-fastest growth rate in the state, with no sign of slowing down. An easy commute from the city, attractive neighborhoods and good schools have helped skyrocket its population to nearly 7,000 residents in recent years.
  • Hydro-Clear® filter: a good neighbor at Julington Creek

    Julington Creek is a 4,200-acre (1,700 hectare) planned community, featuring woodlands, lakes, a library, a recreational facility, and 18 holes of golf.  Developed under Florida’s CDD (Community Development District) program, the community is located in south suburban Jacksonville, close to the east bank of the St. John’s River.
  • Hydro-Clear® sand filter rehabilitation

    The Village of Libertyville, Ill., installed a Hydro-Clear® sand filter system from Evoqua Water Technologies in 1977. Since that time, the Village has benefited from the system, making only minor repairs throughout the years.
  • Innovative cover installed for waste-to-energy purposes

    LaForge Bioenvironmental operates a waste-to-energy facility in a northwest farming community of New Brunswick, Canada. The system is located on a 1,000 acre (405 hectare) mixed farming operation, which includes the LaForge Holsteins dairy.
  • James River Treatment Plant meets odor control commitments

    The James River Treatment Plant is one of nine major treatment plants operated by the Hampton Roads Sanitation District (HRSD), a political subdivision of the Commonwealth of Virginia. Located in Newport News, Virginia, USA, the James River Treatment Plant is committed to protecting the environment and enhancing neighboring communities through a variety of wastewater treatment improvements.
  • Liner helps facility return to its regular operations

    The Remington Water Pollution Control Facility needed a liner replacement for one of its basins because the existing liner was old and damaged. The facility had made arrangements for a liner replacement, but the contractor unexpectedly backed out of the agreement to install the liner before the end of the year.
  • Logan Township, NJ expands water reclamation facility

    Situated on the banks of the Delaware River, Logan Township, New Jersey has a long history of caring for its watershed and natural environment. In the early 70s, the town designed what has been described as “the nation’s first ecologically planned industrial complex,” Pureland Industrial Complex.
  • Marathon wastewater treatment plant meets effluent standards

    Like many cities in the Florida Keys, Marathon, Florida had historically used septic systems to treat wastewater.  The community added secondary treatment several years ago, but the facility was unable to prevent nitrogen and phosphorous contamination of sensitive Gulf of Mexico coastal waters.
  • Massive cover delivers valuable biogas benefits for Melbourne water

    Melbourne Water is a water wholesaler in Victoria, Australia, and is ranked among the top performing Australian and international water utilities. Melbourne Water delivers over 430 billion litres (114 billion gallons) of safe drinking water and treats over 300 billion litres (79 billion gallons) of sewage from across Melbourne.
  • Midas® OCM eliminates odors associated with sewer collection system

    In 2004, a major west coast city began construction of two new interceptor sewers. The 12 foot diameter intercept lines relieve hydraulic overloading, but also created a number of turbulent areas where nuisance odors adversely affected the local residential community. These odors were primarily H2S at concentration levels of up to 150 ppm, as well as volatile organic contaminants (VOCs).
  • Mobile equipment reduces phosphorus in wastewater effluent

    The city of Rosemount, Minnesota, was seeking treatment for phosphorus in the effluent discharge from the city's wastewater treatment plant. The customer's 0.75 MGD facility was permitted to discharge wastewater with a maximum average monthly total phosphorus level of 1.0 mg/l; however the effluent from the facility's newly installed disc filters was exceeding the NPDES permit limit.
  • Mobile water treatment eliminates iron level issues

    This client operates a groundwater treatment facility at a Super Fund site where groundwater is pumped to a VOC stripper for the removal of TCE which is then re-injected into the aquifer. High iron levels in the groundwater caused fouling of pumps, pipes and well casings. This fouling threatened the reliability of the process in terms of flow.
  • Modular cover helps town expand anaerobic sewer lagoon

    ​As part of an upgrade to the town’s wastewater treatment facility, Ranchester was considering an expansion of its existing lagoon infrastructure to include anaerobic pre-treatment. The project involved dividing an existing aerated lagoon into two separate cells.
  • Odor control covers end neighbors’ complaints

    The South Dearborn Regional Sewer District in Lawrenceburg, Indiana, provides regional wastewater treatment services for three cities and an international distillery. The 6 mgd treatment plant is located in an area of high population growth and is surrounded by many retail operations and other commercial developments.
  • OMNIFLO® SBR is key for plant renovation at Hermitage, PA WWTP

    Located in the Shenango Valley watershed of western Pennsylvania, the City of Hermitage's aging infrastructure began to collide with its growing treatment needs. Hermitage also undergoes heavy summer thunderstorms when wastewater volume can double or triple in a couple of hours.