It looks like you are coming from United States, but the current site you have selected to visit is Jordan. Do you want to change sites?

Yes, please. No. Keep me on the current site.

Case Studies

Case Studies

  • Xylem CoMag helps Yorkshire Water exceed phosphorous targets

    Due to a projected population increase, discharges from the site were required to undergo advanced biological treatment to reduce levels of phosphorous returned to the River Aire. This requirement was part of the UK Environment Agency’s Water Industry National Environment Programme (WINEP).
  • CHE enhances flood prevention and management in the Ebro river basin

    Confederación Hidrográfica del Ebro (CHE) deployed an Early Warning System to anticipate river, pluvial and flash events across the 85,000 km² Ebro basin, integrating hydrological and meteorological sensors, rainfall radar and weather forecasts to deliver timely alerts, maps and operational recommendations.
  • Safeguarding water supplies with SmartBall

    In 2020, real water loss in the town’s network peaked at 27 percent. Leaks were undermining the town’s critical water conservation efforts. Recognizing the urgency of the issue, the town is deploying innovative solutions to combat water loss and ensure a sustainable water supply.
  • Dŵr Cymru Welsh Water, Hirwaun Water Treatment Works, Glamorgan

    Dŵr Cymru Welsh Water’s Hirwaun water treatment works is a small works (5Ml/d) which treats raw water from the Penderyn upland reservoir. Treatment is by coagulation with ferric sulphate and lime, flocculation and clarification by DAF. The clarified water is dosed with lime and this is followed by first stage filtration in four rapid gravity filters, intermediate electrochlorination and orthophosphoric acid dosing, and second stage filtration in four pressure filters. Final disinfection is by electrochlorination. The original electrochlorination plant was an Evoqua OSEC® packaged unit installed over twenty years ago and had reached the end of its asset life.
  • City of Tulare celebrates 25 years of converting waste-to-​energy

    The City of Tulare, located in California’s world renowned San Joaquin Valley, is known for its rich agricultural and dairy industries. Tulare is home to six large-scale cheese and dairy producers. Like many municipalities, the city is challenged to meet industrial requirements at a reasonable cost while maintaining harmonious relationships with the surrounding community.
  • CoMag® System Provides Immediate Results

    Situated in Staffordshire in the UK, the Severn Trent Cannock wastewater treatment facility serves a population of 65,053. The plant had early obligation AMP7 requirements to meet for controlling phosphorus levels.
  • Cover helps community control odors from wastewater treatment

    When the affluent, new home development was being established, odor control was top of mind. The wastewater treatment plant was in close proximity to the new development, which includes 900 acres (364 hectares) of preserved open space, including 24 miles (38 kms) of trails, 10 neighborhood parks, a community pool and water park, as well as outdoor sport courts.
  • Cover System Helps Vallejo Sanitation District Streamline Plant Operations

    The Vallejo Sanitation and Flood Control District is an independent special district created by the State of California to collect and treat wastewater and protect the Vallejo community from flooding. Since 1952, the district has protected public health and the San Francisco Bay Area by treating wastewater generated by the more than 115,000 residents of Vallejo and surrounding area.
  • Covers help keep Kamloops beautiful

    The City of Kamloops is located in the interior of British Columbia, Canada’s westernmost province. Situated along the scenic Thompson River, the city’s wastewater treatment facility currently serves a population of over 80,000 people and treats a daily flow of 40,000 m³ (10 mgd), a number which would soon increase to 60,000 m³ (16 mgd).
  • Disc Filtration Solution Helps WWTP Meet Future Clean Water Needs

    About an hour south of Atlanta, the city of Barnesville, Georgia is a town of shady, tree-lined streets, a fondness for celebrating its history, and a sharp eye on the future. In 2013, as its 30-year-old wastewater treatment plant was reaching the end of its useful life, Barnesville found itself planning for a future of growth, progress, and a new, state-mandated <0.6 mg/L total phosphorus (TP) wastewater discharge limit.
  • Everybody wins at Ho-Chunk Casino in Wisconsin

    At the Ho-Chunk Casino owned and operated by the Ho-Chunk Indian Tribe, thousands of people try their luck. However, at the wastewater treatment facility, customers, suppliers, and engineers win.
  • Xylem selected as a supplier for wastewater treatment pilot facility

    The City of Los Angeles has selected Xylem through its sales partner MiscoWATER, to manufacture and install a wastewater treatment system at the Hyperion Water Reclamation Plant. The new treatment system will be installed as part of a pilot facility to evaluate three membrane bioreactor (MBR) systems.