-
Faster draft beer service with Flojet pumps | Bottoms Up System
For GrinOn Industries, creators of the innovative Bottoms Up draft beer dispenser, the goal has always been simple: deliver great beer to people faster, with less waste and zero compromise on quality. -
EMASA: improving water efficiency through smart water balance analysis
EMASA (Empresa Municipal Aguas de Málaga S.A.) is the Malaga City Council’s public utility which has been in charge of managing the entire urban water cycle since 1987. The company serves more than 600,000 residents and supplies approximately 42 hm³ of drinking water. The system operates at a flow rate of up to 2 m³/s, ensuring urban water supply through an extensive pipeline network of around 2,000 km, divided into approximately 240 DMAs (District Metered Areas) and equipped with over 240,000 meters, 170,000 of which are smart devices. -
Gruppo CAP: intelligent water network management through advanced analytics and predictive asset planning
Gruppo CAP deployed Xylem Vue's AI-driven platform to optimize its 6,500 km water network, reducing water losses and improving asset management. -
City of Mesa pinpoints critical leak, avoiding costly delays
Discover how the City of Mesa, Arizona, used Xylem's SmartBall® technology to pinpoint a hard-to-find pipeline leak, safeguarding infrastructure and avoiding costly delays to a transportation project. -
Sörbyvägen Sewage Pumping Station
In conjunction with the expansion of a new pedestrian and cycle path along Route 160, specifically the section between Sörbyvägen and Myggenäs, new water and sewage pipelines were installed. As a vital component of this project, a new sewage pumping station was established to ensure reliable and long-term wastewater management for the area. -
How Fond du Lac turned a nutrient mandate into a smarter operating model
Discover how Fond du Lac met strict phosphorus limits and saved $82K annually by retrofitting with Xylem's biological treatment. Read the case study now. -
Kiski Valley Water Pollution Control Authority: Future-ready wastewater treatment
Discover how Kiski Valley Water Pollution Control Authority upgraded its wastewater treatment system with Sanitaire ICEAS® technology to handle extreme flows, improve efficiency, and protect the Kiski River. -
Regenerative media filter for an outdoor pool
At the Blumenthal outdoor pool in Bremen the Defender regenerative media filter is replacing the outdated, failure-prone open filter system. -
Stadtentwässerung Celle: Wastewater treatment plant process optimization through artificial neural networks
Celle cuts energy consumption by 22% and chemical use by 56% using Xylem Vue WWTP optimization technology, saving tens of thousands of euros annually. -
Powering Singapore’s next generation of semiconductor manufacturing
Xylem delivered a 700 m³/day ultra-pure water system with world-class purity, fast-track execution and built-in capacity for future fab expansion. -
Intake pumping stations P1 and P2 in Kristianstad
As part of Kristianstad Municipality’s investment in a new wastewater treatment plant, construction of two new intake pumping stations – P1 and P2 – began in 2022. The stations play a central role in the facility and are designed to pump wastewater from the trunk sewer network to the new treatment plant. The project was carried out between March 2022 and November 2024. -
Future-proof water supply for the Waldviertel, Austria
EVN Wasser GmbH, the largest water supplier in Lower Austria, implemented a groundbreaking infrastructure project between 2020 and 2025: the new construction of the drinking water Waldviertel pipeline. This 60-kilometre-long main supply pipeline from the Grunddorf/Donaudorf fountain field to Zwettl secures the future supply of high-quality drinking water to around 120,000 inhabitants – an investment in quality of life and future security for an entire region. -
Delivering cost-effective process monitoring for the welding industry
Discover how Sentec engineered a compact, non-intrusive smart connector to digitally transform welding operations. From non-contact wire speed sensing to seamless Bluetooth integration, this case study highlights a scalable solution built for regulation, reliability and industry-wide adoption. -
CCACVI: Acquisition, implementation, hosting and maintenance of a hypervision solution for water and sanitation systems
The French Community of Communes Albères Côte Vermeille Illibéris (CCACVI) is promoting a hypervision project to streamline its water cycle, based on the Xylem Vue platform. -
Innovative water reuse solutions with Xylem’s advanced treatment technology
Learn how Xylem’s Wedeco UV technology helped Los Angeles achieve advanced treatment, regulatory compliance, and 12 MGD of high-quality recycled water at Terminal Island. -
Xylem as turnkey contractor for the new pumping stations in Bromstensstaden
Urban development in Bromstensstaden required new, reliable wastewater pumping stations to meet increased demands on the water and wastewater system. -
Xylem as turnkey contractor for a new pumping station solution in Kristvallabrunn
Xylem delivered a turnkey pumping solution in Kristvallabrunn, including a new pumping station and booster station for reliable, energy-efficient wastewater transfer. -
Satellite manufacturer achieves zero liquid discharge with Xylem
A Texas-based satellite manufacturer solved the challenge of no sewer access by deploying a zero liquid discharge water recycling system. The solution enables 95%+ water reuse, recovers 66M gallons annually, and avoids $30M+ in disposal costs, while digital monitoring ensures reliable, uninterrupted satellite production and strong sustainability performance. -
ApaVital S.A.: Reduction of daily water losses by over 800 m³
ApaVital deploys Xylem Vue to reduce daily water losses by over 800 cubic meters, achieving compliance with EU regulations. -
Predicting failure: smart fault detection for underground cable networks
Sentec partnered with a leading solutions provider to develop a scalable monitoring system that predicts and accurately locates faults in underground cable networks, enabling faster and more cost-effective maintenance. -
Advancing carbon capture: sensor technology to monitor safely and at scale
Discover how Sentec partnered with a leading CCS operator to identify sensor technologies and integration pathways for safe, scalable CO₂ monitoring, enabling safer long‑term storage, reduced operational complexity, and regulatory‑ready deployment strategies. -
Driving precision and sustainability in agri-tech
Learn how Sentec developed calibration free agricultural flow meters in record time boosting accuracy reducing waste improving yields and supporting sustainable farming -
Stadtwerke Trier: AI-aided energy optimization for daily energy balancing
Xylem Vue helped Stadtwerke Trier optimize renewable energy use in its drinking water network, achieving 90% self-consumption. -
Critical pipe repair: Smith-Blair adapters help Canadian sawmill
See how custom Smith-Blair 935/936 adapters repaired deteriorated concrete pipe at a Canadian sawmill without service interruption. Read the full case study.