It looks like you are coming from United States, but the current site you have selected to visit is Iraq. Do you want to change sites?

Yes, please. No. Keep me on the current site.

Xylem Vue Secure Connect: Create a station with TCP XAM 912

Go through the set up wizard to create a station with Nexicon XAM 912 TCP modbus communication. As well how to change the IP address on the CCD 401 Gateway in the set up wizard.