It looks like you are coming from United States, but the current site you have selected to visit is Iraq. Do you want to change sites?

Yes, please. No. Keep me on the current site.

Case Studies

Case Studies

  • OMNIFLO® SBR is key for plant renovation at Hermitage, PA WWTP

    Located in the Shenango Valley watershed of western Pennsylvania, the City of Hermitage's aging infrastructure began to collide with its growing treatment needs. Hermitage also undergoes heavy summer thunderstorms when wastewater volume can double or triple in a couple of hours.
  • OMNIFLO® SBR MAX system expands capacity and addresses flows

    Constructed in the 1980s, the A.J. Brown plant is the largest of three wastewater plants in the city of Huntsville. This upgrade will expand capacity, improve energy efficiency and better handle peak wet weather flows in a small footprint. 
  • Orbal® system selected for new wastewater treatment plant

    Xylem has announced that it has been selected by Payson City, Utah, to expand the City’s wastewater treatment plant. The plant expansion will address the needs of this growing community as well as meet current and future nutrient removal requirements.
  • Prattville addresses treatment capacity and nutrient removal

    Nutrient removal is an important process in meeting high quality effluent requirements. Excessive levels of nitrogen and phosphorous disrupt the natural environment and can affect the health of water systems. Furthermore, Prattville's wastewater system was projected to reach its capacity as the population of the surrounding area grew.
  • Preserving paradise: how a utility in key west is maximizing water reuse

    Key West is one of America’s most scenic locales. Situated in the Florida Keys southwest of Miami, it is visited by millions of people each year and is home to more than 30,000 year-round residents. While there’s plenty of ocean, potable water is a precious commodity which is piped 125 miles from the mainland.
  • Regional Utilities handles growth with the OMNIFLO SBR system

    A forward-thinking not for profit private utility was in need to keep pace with population growth and seasonal flows in a space-constrained, environmentally sensitive resort environment. Walton County, a coastal resort area in northwestern Florida doubles its population during the spring break and summer seasons.
  • Replacement of RBC units will improve treatment performance

    Xylem, an industry leader in mission-critical water treatment solutions, has been selected through a fair and open competitive bidding process to replace eight Rotating Biological Contactors (RBCs) that have reached the end of their useful life at the Cape May County, Municipal Utilities Authority, Cape May Wastewater Treatment Facility.
  • Revamping treatment process to meet discharge limits

    In December 2009, a non-hazardous liquid waste treatment facility in Wisconsin was exceeding their permitted level of 0.165 ppm tin in their final wastewater effluent discharge to the Publicly Owned Treatment Works (POTW). Additionally, effluent levels for lead and copper also approached permit limits and were a concern to this customer.
  • Robesonia – Wernersville Municipal Authority

    Located in Wernersville, Pennsylvania a borough of Berks County, the Robesonia – Wernersville Municipal Authority Wastewater Treatment Facility was prompted to upgrade its filtration process to address two aging traveling bridge sand filters and to meet new state water quality standards, including phosphorus effluent limits.
  • Severn Trent continues to invest in CoMag® systems

    Xylem has been selected by Severn Trent to supply its innovative ballasted clarification technology, the CoMag® system, at yet another major wastewater treatment works. This new contract at Hartshill (near Nuneaton) follows the successful implementation of the CoMag system.
  • Sewerage District relies on PURELAB ® system for BOD testing

    Heart of the Valley Sewerage District in Kaukauna, Wisconsin required high-purity water to test plant effluent for biochemical oxygen demand (BOD) and other contaminants. Testing is required to ensure that the effluent meets state and federal guidelines before discharge into the Fox River.
  • Southwest Water Reclamation Facility – League City, TX

    League City contracted with CDM Smith to manage the expansion project and design and construct a 4.0 MGD (design) / 12 MGD (peak)treatment facility with an energy, labor, and operational efficient process that would meet exceptionally stringent discharge limits. The facility also needed to ensure Type I or Type II non-potable reuse was available for future irrigation and/or amenity use.
  • Bioxide® solution reduces odors, corrosion, and complaints

    Xylem was contacted by a Mid-Atlantic Water Authority to propose an odor control solution at one of their pump stations. The Authority was treating the odors with a sodium hypochlorite (bleach) solution to varying degrees of success. Downstream hydrogen sulfide levels in the atmosphere were the primary contributors to odor complaints, reports of corrosion, and worker safety issues.
  • Alkagen® AQ Solution Provides Point Source Odor and Corrosion Control

    Evoqua Water Technologies LLC was contacted by a South Florida Municipality to provide an odor control solution for a lift station within their collection system. In the past, the municipality had implemented biofiltration for control of atmospheric hydrogen sulfide. However, in recent years the biofilter was removed, leaving the lift station untreated and exposed to high sulfide concentrations.
  • Chain and scraper upgrades help WWTP meet NPDES requirements

    The City of Los Angeles’ Hyperion Wastewater Treatment Plant is one of the largest in the United States. It serves approximately 9 million people by treating 460 mgd of wastewater. Built in 1949, the plant was designed to treat up to 450 mgd but was forced to reduce secondary treatment in the 1960’s to 120 mgd due to limited secondary capacity.
  • Turnkey solution eliminates chain and scraper downtime in Grass Valley, CA

    The Grass Valley Wastewater Treatment Plant provides service for a population of approximately 12,000 people. Situated in California’s Gold Country, the area has some unique challenges that include mine drainage and heavy flows during the winter storm season in the scenic Sierra Nevada foothills. On average, the City discharges 2.1 million gallons per day of treated wastewater effluent to Wolf Creek, a tributary of the Bear River.
  • Meeting stringent phosphorus limits under a wide range of conditions

    The Village of Waterbury Wastewater Treatment Plant (WWTP) is located on the Winooski River floodplain, which poses challenges from significant flooding during the spring runoff and storm seasons to strong algal blooms in late spring. During algal blooms, the plant encounters bright green lagoon effluent high in total suspended solids(TSS), resulting in treatment upsets and inconsistent permit compliance.
  • Town Branch WWTP controls odors with modular covers

    The Town Branch Wastewater Treatment Plant located in Lexington, Kentucky, USA, serves a population of 130,000—about 60% of Lexington—Fayette County. The plant began operating in 1919, and currently treats almost 11 billion gallons of wastewater annually.
  • Xylem to provide a turnkey wastewater treatment solution

    Xylem has been selected by Carolina Water Service, Inc. of North Carolina, through its sales partner Premier Water, to design, manufacture and install a turnkey wastewater treatment system located in the gated golf course community of Brandywine Bay located in Morehead City, N.C.
  • Upper Gwynedd Township, PA. wastewater treatment facility

    The Upper Gwynedd Township, Pennsylvania wastewater treatment plant (WWTP) which treats residential waste (70 percent) and industrial waste (30 percent) was struggling to maintain performance during peak wet weather flows. The facility was designed to treat an average daily flow of 5.7 million gallons per day (MGD) and a maximum monthly flow of 6.5 MGD with a peak hourly flow of 12 MGD.
  • UV disinfection offers a safe and efficient replacement for old process

    The City of Scottsburg is located in Indiana between Louisville, Cincinnati, and Indianapolis. Scottsburg maintains a healthy balance between commercial, industrial and residential community with a celebrated history and bright future. Scottsburg has put a large emphasis on "quality of life" and it shows in their beautiful parks and lively downtown square.
  • UV disinfection systems selected for water reuse growth plan

    The City of Dundee is a growing community with a strong economy boasting three wineries within the city limits and several others in the surrounding Willamette River Valley. The City's existing WWTP was nearing capacity, and the limited discharge to the Willamette River would not adequately support Dundee's planned growth.