The Avensor application currently only supports Google Chrome.
It looks like you are coming from United States, but the current site you have selected to visit is Croatia. Do you want to change site?
Emergency hotline open 24 hours a day (English speaking only): +1 833 677 8776, extension 1
Scroll down to find more information.
No upcoming system maintenance
The Avensor application currently only supports Google Chrome.
Check that you have added a device in the station.
Please check that you have created a call list that is associated to your station. Please also verify that the users in the call list have correct phone numbers for SMS notification.
It means that either the station has lost its mobile connection or that the CCD has no power.
It means that the device is not communicating with the CCD. The communication cable might not be installed correctly, or the settings in the application or the device is not correct (wrong Modbus address or other communication link parameters).
Yes, you have to acknowledge the alarm in the pump controller.
If you go to the alarm tab and look at the top right you can enable and disable various filters in order to active or also ceased alarms.
To connect any device with a digital signal, you need to make sure that there is a +24 V signal.
Below RS232/RS485 communication parameters supported:
Yes, it is possible. Look at below diagram to understand the connection requirements:
The terminal block is designed for stranded and solid wires with an area between 24 and 16 AWG (0, 205 – 1, 31 mm2). Stranded cable shall be striped 7 mm and twined for mounting. The orange spring button must be pressed to bottom before inserting the cable in the terminal blocks. The spring button shall be pressed behind the front surface of the terminal. For this, a tool with a small tip must be used.
The IP/subnet mask for CCD401 is 10.10.10.2/255.255.255.0
Make sure that the device is turned on with network LED solid or blinking green & cloud connection LED is solid or blinking yellow before adding the station in Avensor.
Yes, but this will make Digital input & Digital output non-functional. Use this way only if your setup does not require them.
There are 2 digital outputs supported DO1 & DO2.
Emergency hotline open 24 hours a day (English speaking only): +1 833 677 8776, extension 1
For non-emergency cases, please fill out the form below. A response will be sent within 48 hours.
All fields required.