Search Results
-
FAQ
Everything You Need to Know About Selecting an Aeration Device
Guide for technologies that power the activated sludge process
-
FAQ
FAQs for Gas Feed Systems
Chlorine gas (Cl2) is a highly effective oxidant and a relatively economical option for disinfection. Since Charles F. Wallace and Martin F. Tiernan discovered the first chlorine gas feed system in 1913 the Wallace & Tiernan® brand is a synonym for safe and reliable disinfection of water. Chlorine can be safely transported, easily applied, measured, and controlled. See below for more frequently asked questions regarding Gas Feed disinfection.
-
FAQ
How to Maximize Clarifier Performance
Clarifiers are an important component of the wastewater treatment process. However, between corrosion, maintenance, and changes in flow, it can be difficult to keep a clarifier operating at peak performance. In addition, changes in effluent regulations may require upgrades to meet new, more stringent requirements. To learn more about clarifiers and their maintenance, Allen Lepak, Clarification Product Manager with Evoqua Water Technologies provides expert advice on how to identify some common issues with clarifiers, how to maximize performance, and how to decide whether you should upgrade or replace your existing unit.
-
FAQ
Zero liquid discharge (ZLD) FAQ for Xylem’s Vacom One-Step
Get answers on ZLD cost, pretreatment, reliability, fouling control, and installation timeline. Learn how Xylem’s Vacom One-Step simplifies ZLD. -
Activated sludge challenges video series
Learn how EnviroMix’s FlexZone system optimizes activated sludge processes. -
Flygt
Vortex Impeller D 3060
-
Flygt
Vortex Impeller D 3127
-
Bringing pumping efficiency beyond par
England’s Northumbrian Water Ltd (NWL) serves roughly 2.5 million people with water and sewerage services. To better assess its predicted results they conducted a project to measure how much the installation of N-pumps had reduced their costs.
-
CCACVI: Acquisition, implementation, hosting and maintenance of a hypervision solution for water and sanitation systems
The French Community of Communes Albères Côte Vermeille Illibéris (CCACVI) is promoting a hypervision project to streamline its water cycle, based on the Xylem Vue platform. -
City of Kaufbeuren: increasing energy and resource efficiency through AI-based process control
In the face of climate change and cost and supply uncertainties, cities and municipalities must operate their plants and processes as efficiently and sustainably as possible. In this context, the town of Kaufbeuren recognized significant potential for energy optimization at its wastewater treatment plant.
-
Clayton County, Georgia reduces apparent water loss & identifies one million in recoverable revenue
Clayton County Water Authority (CCWA) is a good example of a utility that doesn’t let a confined geographical footprint stop it from thinking outside the box. As one of Georgia’s smallest counties in terms of land size area (only 143 square miles), its location near the top of a regional watershed means it has little area to gather precipitation into streams and rivers.
-
Cover helps community control odors from wastewater treatment
When the affluent, new home development was being established, odor control was top of mind. The wastewater treatment plant was in close proximity to the new development, which includes 900 acres (364 hectares) of preserved open space, including 24 miles (38 kms) of trails, 10 neighborhood parks, a community pool and water park, as well as outdoor sport courts.
-
EnviroMix BioCycle-D delivers 45% energy savings in Adairsville, GA
Read how Adairsville’s North WWTP reduced aerobic digestion energy use with EnviroMix BioCycle-D by decoupling aeration from mixing and using automated aerobic and anoxic cycles, delivering more than 45% energy savings versus conventional diffused air mixing. -
EnviroMix BioCycle-D delivers AL plant low-maintenance aerobic digestion
Read how the Eastside Wastewater Treatment Plant in Albertville, AL used the EnviroMix BioCycle-D™ process to simplify operations, reduce maintenance, and improve energy efficiency. -
EnviroMix BioCycle-D helps WRF meet phosphorus limits in Detroit Lakes, MN
Read how Detroit Lakes, Minnesota met a 0.066 mg/L phosphorus limit by upgrading aerobic digestion with EnviroMix BioCycle-D, delivering 77% energy savings and over $100,000 in annual power cost savings while keeping phosphorus sequestered in the sludge. -
EnviroMix BioMix enhances BNR and reduces DO in Orlando, FL
See how Orlando’s Water Conserv II WRF improved denitrification by replacing diffused-air mixing with EnviroMix BioMix to lower dissolved oxygen in anoxic basins, reduce long-term O&M costs, and strengthen BNR performance and resiliency after high-flow events. -
EnviroMix BioMix helps HRSD keep Chesapeake Bay clean
Read how HRSD used EnviroMix BioMix™ technology to improve biological nutrient removal, increase operational flexibility, and reduce O&M costs at the VIP Wastewater Treatment Plant. -
EnviroMix BioMix provides O&M savings in Russellville, AR
See how Russellville’s Pollution Control Works reduced operating costs with BioMix compressed gas mixing and achieved 75% energy savings in Phase I and more than 60% in Phase II versus mechanical mixers. -
EnviroMix BioMix reduces O&M costs in Henderson, CO
See how SACWSD’s Williams Monaco WWTP reduced O&M demands by replacing submersible mixers with EnviroMix BioMix compressed gas mixing, delivering 50%+ energy savings for anoxic and anaerobic selectors. -
Xylem's SBR System Installed at Bowling Green, Kentucky
Bowling Green Municipal Utilities (BGMU) provides commercial water and wastewater treatment and electrical power services to a population of more than 60,000 in the community of Bowling Green, KY. In 2010, the BGMU wastewater treatment plant was approaching the end of its useful life, just as the utility’s operating permit was up for renewal.
-
EWE WASSER GmbH: application of a real-time assistance system to reduce aeration energy usage and minimize operational expenses
Xylem Vue has helped to reduce Cuxhaven’s WWTP aeration energy requirements by over 26% and meet its effluent quality requirements.
-
Flygt Concertor eradicates wastewater pump blockages for Yorkshire Water
Yorkshire Water’s Dynamic Maintenance Team identified that they required an easily deployable solution that delivered tangible benefits across the network.
-
Innovative cover installed for waste-to-energy purposes
LaForge Bioenvironmental operates a waste-to-energy facility in a northwest farming community of New Brunswick, Canada. The system is located on a 1,000 acre (405 hectare) mixed farming operation, which includes the LaForge Holsteins dairy.
-
Landfill leachate treatment system significantly reduces operations cost
The South Central Counties Solid Waste Agency, located in Hopewell, Pennsylvania needed a cost effective, on-site treatment system to treat 12,500 gpd of leachate and allow for future expansion.