It looks like you are coming from United States, but the current site you have selected to visit is Georgia. Do you want to change site?

Yes, please! No, keep me on the current site

How one Florida utility is benefiting from a state-of-the-art management tool

USA

To learn about Royal Palm Beach's SCADA system, read the article.

"Now instead of driving to a lift station, the field force can remotely reset a motor and analyze the cause of failures from the CMF.."

"The data can forewarn of impending problems with motors, electrical supply or potential blockages that serve as the basis for proactive maintenance.."

"The Multitrode Outpost system is easy to manage because it comes preconfigured with built-in expansion capabilities via pop-up screens.."

Download Case study