It looks like you are coming from United States, but the current site you have selected to visit is Georgia. Do you want to change site?

Yes, please! No, keep me on the current site

Sewer bypass solution delivered in France in one week

Sewer bypass solution delivered in France in one week

When connecting a new wastewater treatment plant in France to the sewer, a temporary bypass solution was needed for the old treatment plant. Xylem delivered a turnkey bypass solution in just one week, using its extensive rental fleet of Godwin pumps. 

In October 2014, construction work began on a new municipal wastewater treatment plant in Mainvilliers, France, located southwest of Paris. The new wastewater treatment plant was designed to replace an existing plant located in nearby Lèves, which had been in operation since 1948. The old plant served 160,000 residents from both Mainvilliers and Lèves, as well as the surrounding municipality of Chartres. Due to aging infrastructure and increased demand, however, the plant was no longer fit for purpose.

Bypass needed when connecting new sewer inlet

When construction work on the new wastewater treatment plant was drawing to a close in April 2017, Sade, the company supporting the construction project on the sewer, began the challenging task of connecting the existing sewer inlet at the plant in Lèves to the new station in Mainvilliers. Extensive works had to be carried out on the Lèves plant’s main manifold, which required the diversion of incoming wastewater to allow for the works to take place. A temporary bypass pumping solution was needed to properly manage the wastewater flow and to allow the pumping station to continue to operate without disruption.

Xylem delivers customized bypass solution

Sade engaged leading global water technology company Xylem to provide a solution, leveraging the company’s comprehensive dewatering portfolio and application expertise to carry out the project. Xylem deployed an expert team of engineers to work alongside Sade, delivering a customized bypass solution in record time.

As the old wastewater plant at Lèves dealt with particularly high volumes of wastewater, the new bypass solution needed to withstand a maximum flow level of 2,680 cubic meters per hour (m3/h). Flow levels at Lèves would vary day to day depending on user demands and fluctuating precipitation. For this reason, a flexible solution capable of handling flow variations and dealing with peak volumes was required.

Xylem proposed a state-of-the-art, environmentally-friendly rental dewatering solution that would offer the quickest turnaround time to complete the task and be cost efficient. Using the company’s strong footprint in the region, Xylem was able to deliver the complex bypass application without delay. Xylem has more than 6,000 rental assets available to European customers at nearly 80 rental sites. This allows the company to position the right fleet mix in the right location, at the right time to support customer needs with temporary and long-term rental solutions.

Rental dewatering solution offers reliability and peace of mind

Xylem’s dewatering engineers installed a turnkey bypass solution to maintain the sewer line, a project that was delivered in just one week while minimizing environmental impact and ensuring regulatory compliance.

The team supplied two Godwin CD225M diesel pumps along with one Godwin Dri-Prime CD400M pump. The combination of diesel pumps allowed the temporary bypass to operate at maximum efficiency, offering a flexible solution for fluctuating wastewater flow levels. The pumps can handle a capacity up to 1,700 m3/h – giving a total combined flow of 2,700 m3/h across the three pumps. This flow level exceeded the maximum flow level of 2,680 m3/h usually experienced by the wastewater plant and ensured that the bypass had sufficient capacity to withstand varying flow levels caused by increased user activity or precipitation.

The Godwin pumps were fitted with variable frequency drives (VFD), enabling operators to control the motor speed and reach the required duty point, ensuring optimum operating efficiency throughout the project.

The diesel pump model used for this project also has the capacity to handle solids up to 75 millimeters (mm) in diameter, allowing small, fibrous materials to pass through the pump’s impeller with ease. This, along with the portability of the pump, makes it an excellent choice in challenging dewatering applications where sewage, sludge, or unwanted water need to be removed or redirected.

To support the bypass, Xylem supplied twelve 400 mm pipes, measuring 3 meters in length, to safely channel the discharge of wastewater away from a nearby river and avoid environmental damage. Xylem’s Godwin pumps were equipped with Tier 4 diesel engines, which reduce air pollution by minimizing the discharge of particulate matter and nitrogen oxides in the air, as well as providing enhanced engine control and reduced noise.

Bertrand Pasquier, Head of SADE Normandy, said, “Xylem’s support during the 15-day bypass operation allowed us to meet the specifications of the project in record time. Drawing resources from its European network of rental hubs, Xylem deployed the necessary equipment and expertise quickly and efficiently, enabling us to deliver a reliable solution to the end-customer while ensuring continuous service. Xylem is a trusted partner and the team was integral to the success of the bypass application.”

by Chad Henderson